Skip to main content
Associate II
Dec 28, 2024 5:13 PM UTC
Solved

How to produce list of pin assignments?

Hello, all,

I'm using STM32CubeIDE to design my first STM32 micro-controller circuit. I've used the tool to assign functions to about 20 pins on the micro-controller so far. Now, I'm at the stage where I'm creating the schematic and connecting external circuitry to the micro-controller pins.

Is there an easy way to get a list of the pins I've assigned so far, along with User Labels, so I can go right down the list and wire up the circuits? What I'm doing so far is to keep the STM32CubeIDE open on one monitor and view the pin-out view, and work my way around the chip, wiring pins as I go. Is this the most efficient way to work? Is this how most others do it? I wondered if I was overlooking some built-in function of STM32CubeIDE to perform this task.

Thanks for your advice and suggestions.

-Kevin

 

This topic has been closed for replies.
BTurc.2
BTurc.2Best answer
Senior
Dec 28, 2024 6:01 PM UTC

Hello Kevin,
Personally, when I'm wiring my project in KiCad, for example, I have both STM32CubeIDE and KiCad open. However, if you want to have an Excel spreadsheet with the pinout, you can do the following:
Go to .ioc->Pinout->Export Pinout without Alt. Functions
Captura pantalla.png

 

And you will have an .csv file like this one:
Exel.png

I hope this is what you were searching for.

Have a nice day!

 

4 replies

BTurc.2
BTurc.2Best answer
Senior
Dec 28, 2024 6:01 PM UTC

Hello Kevin,
Personally, when I'm wiring my project in KiCad, for example, I have both STM32CubeIDE and KiCad open. However, if you want to have an Excel spreadsheet with the pinout, you can do the following:
Go to .ioc->Pinout->Export Pinout without Alt. Functions
Captura pantalla.png

 

And you will have an .csv file like this one:
Exel.png

I hope this is what you were searching for.

Have a nice day!

 

Associate II
Dec 28, 2024 7:09 PM UTC

STM32CubeMX has a tool that exports a schematic symbol of your pin assignments. 
You can check section 4.17 of the CubeMX Manual: 
https://www.st.com/resource/en/user_manual/um1718-stm32cubemx-for-stm32-configuration-and-initialization-c-code-generation-stmicroelectronics.pdf

I've had varying degrees of success with larger pinout chips, but I think smaller projects should work just fine. 

KevinZAuthor
Associate II
Dec 30, 2024 5:42 PM UTC

@BTurc.2and @halfordC , thank you both for your helpful replies.

@BTurc.2, that was exactly what I was asking for. Thanks, also, for describing how you work efficiently.

@halfordC, thanks about the schematic output. I'm using KiCAD and might try this, just to experiment. I would have never learned about this on my own.

-Kevin

Andrew Neil
Super User
Aug 4, 2025 8:19 AM UTC

See also: Is a database or metadata pin alternative functions available?

It seems there is (now) a GitHub repository of such info...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.