Skip to main content
GFeke.1
Visitor II
November 14, 2020
Question

How to make LwIP work with CMSIS_V2 in CubeIDE?

Hi,

I have a Nucleo-F439ZI board and I am trying to make a simple application that echoes back a message on a UDP port.

When I generate a project using LwIP raw API, I am able to make that happen with a callback function and a PCB.

However, as soon as I turn CMSIS_V2 RTOS on in the CubeMX configuration perspective and create a few threads (e.g. blinking 2 different LEDs periodically), the execution of the program freezes right after MX_LWIP_Init() is called in "Default thread". I don't even have a chance to initialize a Netconn structure to listen for incoming packets or anything.

If I comment it out, every thread runs as expected, but with thi LwIP initialization function called, the whole execution freezes.

I was wondering if I am missing some trivial step , or this isn't the right way to use LwIP with RTOS, but I am clueless here, since this is the auto-generated code that doesn't work.

Also, in debug mode I get no HardFault or Exception or anything, it seems that the code is running as normal, but the threads are completely frozen.

When MX_LWIP_Init() is called in default thread, every task is frozen.

void StartDefaultTask(void *argument)
{
 /* init code for LWIP */
 //MX_LWIP_Init();
 /* USER CODE BEGIN 5 */
 /* Infinite loop */
 for(;;)
 {
		HAL_UART_Transmit(&huart3, "Hello", 6, 1000);
	 osDelay(1000);
 }
 /* USER CODE END 5 */
}
void StartTask02(void *argument)
{
 /* USER CODE BEGIN StartTask02 */
 /* Infinite loop */
 for(;;)
 {
	 HAL_GPIO_TogglePin(LD1_GPIO_Port, LD1_Pin); //toggle running led
	 osDelay(500);
 }
 /* USER CODE END StartTask02 */
}

I would really appreciate if someone could tell mewhat I am doing wrong.

This topic has been closed for replies.

1 reply

BB s.11
Visitor II
June 25, 2021

I guess that you have the same problem, please check the following:

The parameter LWIP_RAM_HEAP_POINTER = 0x30044000 ("LWIP" category, "Key Options" tab). This memory is probably not accessible on your CPU and the MX_LWIP_Init() fails exactly here:

MX_LWIP_Init() -> tcpip_init( NULL, NULL ) -> lwip_init() -> mem_init() -> fails during the first try to write to the "mem" variable

Solution: You have to find a different memory section that is accessible by this peripheral.