Skip to main content
Associate II
April 13, 2024
Question

How to interface STM32H750xB with ST-Link/V2 debugger

I want to interface STM32H750xB with ST-Link/V2 debugger using TAG connector 
TAG-Connect™ Pin-Out
The Tag-connect provides SWD, USART and USB interfaces for debug, control, and
monitoring the MCU. Table 1 provides TAG-connect connector DBG1 pin-out details.
Pin Signal Name Description
1  VCC3                      +3.3V SOM power supply
2  NRST                      System reset
3  SWCLK/JTCK          Serial wire clock/JTAG test clock
4  SWDIO/JTMS          Serial wire data in/out//JTAG test mode select
5  USART1_TX            USART1 Transmit data
6  USART1_RX            USART1 Receive data
7  USB_FS1_VBUS      USB FS OTG port 1 VBUS input
8  USB_FS1_DM          USB FS OTG port 1 data - line
9  USB_FS1_DP           USB FS OTG port 1 data + line
10  GND                      SOM ground

    This topic has been closed for replies.

    4 replies

    AScha.3
    Super User
    April 13, 2024

    You write > How to i interface STM32H750xB with ST-Link/V2 <

    and then show the interface you want to use (or build a new board ?) - fine.

    And whats the problem then ?

    If you feel a post has answered your question, please click on " Best Answer ".
    MM..1
    Super User
    April 13, 2024

    In normal situation required is pins 10,3,4

    good is add too 2.

    DeepakYAuthor
    Associate II
    April 13, 2024

    But as per what i know pin 3 (JTCK) is for clock And pin 4 (JTMS) for mode selection so we need other pins to transmit and receive data i.e USART1 Tx and Rx 

    I have only worked on boards which have inbuilt stlink so it would automatically generate code in cube ide 

    so i have no idea how to write a code for it so any references would be helpful 

    Thank You

    MM..1
    Super User
    April 13, 2024

    Used signals is SWCLK SWDIO and i dont understand your Q about code. Working with code is exatly same.

    Connect STLinkv2 USB to PC run IDE and use it.