Skip to main content
Associate
Dec 10, 2024 7:18 PM UTC
Question

How to get CubeIDE version for MacOS 12.7 Monterey (Intel)

1. Which CubeIDE version is the latest that supports MacOS 12.7 Monterey for the Intel-based Macs?

2. Where do I go to download it?

Thanks

This topic has been closed for replies.

2 replies

Ghofrane GSOURI
ST Technical Moderator
Dec 11, 2024 8:21 AM UTC

Hello @noName123 

 I recommend using the latest STM32CubeIDE 1.17.0, which supports the following operating systems and architectures:

  • Windows: Windows® 10 and 11 (64-bit)
  • Linux: Ubuntu® LTS 22.04, LTS 24.04, and Fedora® 40
  • macOS: macOS® 14 (Sonoma) and macOS® 15 (Sequoia)

Please note that while STM32CubeIDE may work on macOS 12.7, it is not officially supported on this version. Therefore, to ensure proper functionality on macOS 12.7, I recommend using a virtual machine (VM) with one of the supported operating systems listed above.

You can download the latest STM32CubeIDE from this LINK 

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
noName123Author
Associate
Dec 12, 2024 3:55 PM UTC

Thank you for your reply.

Do any earlier versions of CubeIDE support MacOS 12.7?

I've had bad experience using a virtual machine with other tools and would rather use an earlier version of CubeIDE if there is one that supports my OS.