Skip to main content
Associate III
Mar 4, 2025 11:46 AM UTC
Solved

How to fix this error will not fit in region `RAM_D1'

17:13:32 **** Incremental Build of configuration Debug for project LVGE_ex_code_H7 ****

make -j4 all

arm-none-eabi-gcc -o "LVGE_ex_code_H7.elf" @"objects.list" -mcpu=cortex-m7 -T"D:\stm32H7\LVGE_ex_code_H7\STM32H750VBTX_FLASH.ld" --specs=nosys.specs -Wl,-Map="LVGE_ex_code_H7.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group

C:/ST/STM32CubeIDE_1.14.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: LVGE_ex_code_H7.elf section `.bss' will not fit in region `RAM_D1'

C:/ST/STM32CubeIDE_1.14.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.1.0.202410251130/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: region `RAM_D1' overflowed by 488072 bytes

collect2.exe: error: ld returned 1 exit status

make: *** [makefile:125: LVGE_ex_code_H7.elf] Error 1

"make -j4 all" terminated with exit code 2. Build might be incomplete.

 

17:13:35 Build Failed. 3 errors, 0 warnings. (took 3s.49ms)

 

 

 

/*
******************************************************************************
**
** File : LinkerScript.ld (debug in RAM dedicated)
**
** Author : STM32CubeIDE
**
** Abstract : Linker script for STM32H7 series
** 1024Kbytes RAM_EXEC and 544Kbytes RAM
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used.
**
** Target : STMicroelectronics STM32
**
** Distribution: The file is distributed as is, without any warranty
** of any kind.
**
*****************************************************************************
** @attention
**
** Copyright (c) 2024 STMicroelectronics.
** All rights reserved.
**
** This software is licensed under terms that can be found in the LICENSE file
** in the root directory of this software component.
** If no LICENSE file comes with this software, it is provided AS-IS.
**
****************************************************************************
*/

/* Entry Point */
ENTRY(Reset_Handler)

/* Highest address of the user mode stack */
_estack = ORIGIN(DTCMRAM) + LENGTH(DTCMRAM); /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */

/* Specify the memory areas */
MEMORY
{
 RAM_EXEC (xrw) : ORIGIN = 0x24000000, LENGTH = 1024K
 DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
 RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
 RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
 ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}

/* Define output sections */
SECTIONS
{
 /* The startup code goes first into RAM_EXEC */
 .isr_vector :
 {
 . = ALIGN(4);
 KEEP(*(.isr_vector)) /* Startup code */
 . = ALIGN(4);
 } >RAM_EXEC

 /* The program code and other data goes into RAM_EXEC */
 .text :
 {
 . = ALIGN(4);
 *(.text) /* .text sections (code) */
 *(.text*) /* .text* sections (code) */
 *(.glue_7) /* glue arm to thumb code */
 *(.glue_7t) /* glue thumb to arm code */
 *(.eh_frame)
 *(.RamFunc) /* .RamFunc sections */
 *(.RamFunc*) /* .RamFunc* sections */

 KEEP (*(.init))
 KEEP (*(.fini))

 . = ALIGN(4);
 _etext = .; /* define a global symbols at end of code */
 } >RAM_EXEC

 /* Constant data goes into RAM_EXEC */
 .rodata :
 {
 . = ALIGN(4);
 *(.rodata) /* .rodata sections (constants, strings, etc.) */
 *(.rodata*) /* .rodata* sections (constants, strings, etc.) */
 . = ALIGN(4);
 } >RAM_EXEC

 .ARM.extab (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 *(.ARM.extab* .gnu.linkonce.armextab.*)
 } >RAM_EXEC
 .ARM (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 __exidx_start = .;
 *(.ARM.exidx*)
 __exidx_end = .;
 } >RAM_EXEC

 .preinit_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 PROVIDE_HIDDEN (__preinit_array_start = .);
 KEEP (*(.preinit_array*))
 PROVIDE_HIDDEN (__preinit_array_end = .);
 } >RAM_EXEC

 .init_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 PROVIDE_HIDDEN (__init_array_start = .);
 KEEP (*(SORT(.init_array.*)))
 KEEP (*(.init_array*))
 PROVIDE_HIDDEN (__init_array_end = .);
 } >RAM_EXEC

 .fini_array (READONLY) : /* The READONLY keyword is only supported in GCC11 and later, remove it if using GCC10 or earlier. */
 {
 PROVIDE_HIDDEN (__fini_array_start = .);
 KEEP (*(SORT(.fini_array.*)))
 KEEP (*(.fini_array*))
 PROVIDE_HIDDEN (__fini_array_end = .);
 } >RAM_EXEC

 /* used by the startup to initialize data */
 _sidata = LOADADDR(.data);

 /* Initialized data sections goes into RAM, load LMA copy after code */
 .data :
 {
 . = ALIGN(4);
 _sdata = .; /* create a global symbol at data start */
 *(.data) /* .data sections */
 *(.data*) /* .data* sections */

 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */
 } >DTCMRAM AT> RAM_EXEC

 /* Uninitialized data section */
 . = ALIGN(4);
 .bss :
 {
 /* This is used by the startup in order to initialize the .bss section */
 _sbss = .; /* define a global symbol at bss start */
 __bss_start__ = _sbss;
 *(.bss)
 *(.bss*)
 *(COMMON)

 . = ALIGN(4);
 _ebss = .; /* define a global symbol at bss end */
 __bss_end__ = _ebss;
 } >DTCMRAM

 /* User_heap_stack section, used to check that there is enough RAM left */
 ._user_heap_stack :
 {
 . = ALIGN(8);
 PROVIDE ( end = . );
 PROVIDE ( _end = . );
 . = . + _Min_Heap_Size;
 . = . + _Min_Stack_Size;
 . = ALIGN(8);
 } >DTCMRAM

 /* Remove information from the standard libraries */
 /DISCARD/ :
 {
 libc.a ( * )
 libm.a ( * )
 libgcc.a ( * )
 }

 .ARM.attributes 0 : { *(.ARM.attributes) }
}

 

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 4, 2025 12:44 PM UTC

@Kai_Satone wrote:

@mƎALLEm 
STM32H750VBTX_FLASH.ld

MEMORY

{

FLASH (rx) : ORIGIN = 0x90000000, LENGTH = 8M

DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K

RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K

RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K

RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K

ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K

}

This was not the same linker content you shared in the first post!!

Again, double check your map file (.map) and find what you need to locate in RAM_D1 (the objects that are located in the range 0x2400 0000 -  0x2407 FFFF). relocate the variables or tables etc.. that are not needed to be in the AXI-SRAM (RAM_D1) in other SRAMs (for example in RAM_D2).

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

10 replies

Ozone
Principal
Mar 4, 2025 11:52 AM UTC

> ... region `RAM_D1' overflowed by 488072 bytes

Rethink you strategy of RAM usage, i.e. variables and buffer usage.
In other words, your code must get along with the RAM resources the MCU actually has.

mƎALLEm
ST Technical Moderator
Mar 4, 2025 11:58 AM UTC

Hello,

You didn't provide much information but according to this trace:

`RAM_D1' overflowed by 488072 bytes

You exceeded the usage of that RAM, I think AXI-SRAM. But from the linker file you shared I don't see any definition of RAM_D1:

MEMORY
{
 RAM_EXEC (xrw) : ORIGIN = 0x24000000, LENGTH = 1024K
 DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
 RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
 RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
 ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}

RAM_EXEC (AXI-SRAM) size is incorrect: 1MB!! It should be 512kB:

From the datasheet:

mALLEm_0-1741089449619.png

Check also your map file and find what needs to be located in that memory and what is not.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate III
Mar 4, 2025 12:14 PM UTC

@mƎALLEm  @Andrew Neil 

I have tried your solution but it didn't worked con you tell me what additional information do you need so I can provide you

mƎALLEm
ST Technical Moderator
Mar 4, 2025 12:32 PM UTC

The solution I provided is just one thing among others.

You need to check your map file and find what needs to be located in that memory and what is not to that RAM_D1. You clearly exceeded that memory size. You need to review your memory mapping.

Also you still not answered that question: where you did declare that RAM_D1?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Mar 4, 2025 12:11 PM UTC

@Kai_Satone wrote:

region `RAM_D1' overflowed by 488072 bytes


"overflowed by 488072 bytes" means that you've tried to put 488072 bytes more into that area than it can hold.

So you either need to increase the size of the area, or reduce the amount of stuff you're putting into it - or both!

 

As @mƎALLEm said, your posted linker script does not define any "RAM_D1" - so perhaps just defining it with the appropriate size is all that's needed?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.