Skip to main content
Chris F
Associate
December 5, 2021
Solved

How to fix linker error with atomic compare_exchange_weak

I have an atomic variable and want to use compare_exchange_weak on it.

But I'm getting the following linker error when compiling with STM32CubeIDE v1.8.0 (arm-none-eabi 9.3.1:(

arm-none-eabi\bin\ld.exe: ./Core/Src/main.o: in function `std::__atomic_base<unsigned char>::compare_exchange_weak(unsigned char&, unsigned char, std::memory_order, std::memory_order)':
arm-none-eabi\include\c++\9.3.1\bits/atomic_base.h:457: undefined reference to `__atomic_compare_exchange_1'

Here is a minimal example to demonstrate the linker error:

/* main.cpp */
 
#include <cstdint>
#include <cstdio>
#include <atomic>
 
int main() {
	std::atomic<uint8_t> some_atomic_var { 0 };
 
	some_atomic_var.store(3U); // atomic store works fine
	printf("%u\n", some_atomic_var.load()); // atomic load works fine
 
	auto val = some_atomic_var.load();
 
	// set second bit
	while (!some_atomic_var.compare_exchange_weak(val, val | (1 << 2U))); // gives linker error
	printf("%u\n", some_atomic_var.load()); 
 
	return 0;
}

 Update 6.12.2021:

Platform:Windows version of CubeIDE 1.8.0

STM32 target: STM32F030CC

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
December 6, 2021

Internet wisdom says that you should link -latomic in that case, but I cannot find it in the STM32 release.

otoh, Cortex-M0 is so simple. Are you using multi tasking? If so, check the implementation in RIOT OS https://github.com/RIOT-OS/RIOT/blob/master/core/atomic_c11.c for adding the missing function. If not, you could further simplify it.

Did you write that code or is it meant to be super portable, e.g. for multi-core, out-of-order execution CPUs?

hth

KnarfB

7 replies

KnarfB
Super User
December 6, 2021

Hmm. It links here without errors:

10:30:16 **** Incremental Build of configuration Debug for project atomic ****
make -j12 all 
arm-none-eabi-g++ "../Core/Src/main.cpp" -mcpu=cortex-m4 -std=gnu++14 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32L432xx -c -I../Core/Inc -I../Drivers/STM32L4xx_HAL_Driver/Inc -I../Drivers/STM32L4xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32L4xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -fno-exceptions -fno-rtti -fno-use-cxa-atexit -Wall -fstack-usage -MMD -MP -MF"Core/Src/main.d" -MT"Core/Src/main.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Core/Src/main.o"
arm-none-eabi-g++ -o "atomic.elf" @"objects.list" -mcpu=cortex-m4 -T"STM32_workspace\atomic\STM32L432KCUX_FLASH.ld" --specs=nosys.specs -Wl,-Map="atomic.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group
Finished building target: atomic.elf
 
arm-none-eabi-size atomic.elf 
arm-none-eabi-objdump -h -S atomic.elf > "atomic.list"
arm-none-eabi-objcopy -O binary atomic.elf "atomic.bin"
 text	 data	 bss	 dec	 hex	filename
 5848	 116	 1600	 7564	 1d8c	atomic.elf
Finished building: default.size.stdout
 
Finished building: atomic.bin
Finished building: atomic.list

Chris F
Chris FAuthor
Associate
December 6, 2021

Thanks a lot for trying it out!

Did you use STM32CubeIDE v1.8.0 (also tried it with 1.7.0) and are you using the Windows version of the CubeIDE?

KnarfB
Super User
December 6, 2021

Yes and yes.

gcc version 9.3.1 20200408 (release) (GNU Tools for STM32 9-2020-q2-update.20201001-1621)