Skip to main content
Associate
September 18, 2024
Solved

How to find the CubeIDE on my Mac?

  • September 18, 2024
  • 3 replies
  • 1347 views

After I installed the CubeIDE (STM32CubeIDE-Mac) on my mac with the delivered iinstaller, I cannot find the CubeIDE what is the name of the application? in which folder it is installed?

This topic has been closed for replies.
Best answer by burghard

The Solution to this was the the PKG Archive consists of two things - an installer for a server application which I executed and an application file wich has to be copied into te application folder. 
this file was hides by the lower border of the window in which the contents of the PKG file. So I missed to copy it. After I did I have been able to find the IDE on my computer (-:

May be that the settings for the size of the icons in the finder on my computer ist the reason for my mistake. 

 

3 replies

Andrew Neil
Super User
September 18, 2024

On windows, you can just search for it - does Mac not have that??

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Visitor II
September 19, 2024

It should be in /Applications/STM32CubeIDE.app

It may ask you to download the st-link server, when you run the debugger. Download that from
https://www.st.com/en/development-tools/st-link-server.html
and unzip it and run the mac installer .pkg file in there. On my machine, that installs /usr/bin/local/stlink-server

However, since updating to macOS 15.0 Sequoia, the IDE can no longer find the st-link-server.
https://community.st.com/t5/stm32-mcus-boards-and-hardware/st-link-server-is-required-error-after-macos-update/m-p/719798#M21344
https://stackoverflow.com/questions/78996974/stm32cubeide-debugger-no-longer-works-in-macos-15-0-sequoia

I still don't have mine working. Good Luck!

burghardAuthorBest answer
Associate
September 26, 2024

The Solution to this was the the PKG Archive consists of two things - an installer for a server application which I executed and an application file wich has to be copied into te application folder. 
this file was hides by the lower border of the window in which the contents of the PKG file. So I missed to copy it. After I did I have been able to find the IDE on my computer (-:

May be that the settings for the size of the icons in the finder on my computer ist the reason for my mistake.