How to configure virtual COM using G0B1RE? Windows driver needed?
Hi.
I am working on an application using the USB Virtual COM of the G0B1RE. In the Connectivity option, I enabled the USB_DRD_FS in Device_Only (FS) mode, and in Middleware I configured the USB_DEVICE option as Communication Device Class (Virtual COM).
I tried to run a simple communication test just by sending a message through the CDC_transmit_FS function:
-------------------------------------------------------------
uint8_t bufferTX [] = "TEST USB";
CDC_Transmit_FS(bufferTX, sizeof(bufferTX));
HAL_Delay(1000);
--------------------------------------------------------------
The problem encountered is that Windows did not recognize the Virtual COM, giving the following message: "USB DEVICE NOT RECOGNIZED".
Could someone help me? Do I need to install any driver in Windows 10 to recognize Virtual COM?