Skip to main content
mikew67
Associate II
September 10, 2023
Question

How to build the hsdatalog app from FP-SNS-DATALOG1 project code using STM32Cube IDE

Newbie with STM32CubeIDE here, so apologies if this is a trivial question ;)

How do I use the sample Project code in the FP-SNS-DATALOG1 repo to build the hsdatalog application for the STWIN Starter Kit, STEVAL-STWINKT1B (SensorTile Wireless Industrial Mode)?

  1. I've tried to create a project in STM32CubeIDE v1.13.1 using the code located in the fp-sns-datalog1 repo (tag main.v1.5.0)  in the folder at: /fp-sns-datalog1/Projects/STM32L4R9ZI-STWIN/Applications/HSDatalog/STM32CubeIDE
  2. I've tried several choices of how to load a project into the iDE without success.
  3. Note that the above mentioned folder does not contain an .ioc file
  4. When I attempt to build the app, I get an error: "make: *** No rule to make target"
  5. The "Getting started" doc, skips over this, saying just build the app and proceed.

I probably don't need to rebuild this app -- pre-built binaries are provided and I can exercise the kit using them with json config files, but I definitely prefer to be able to examine and build the code I use.  And I also want to use the STM32Cube IDE vs the alternatives.

So, what do I need to do to load and build the referenced project?

TIA,

Mike

 

This topic has been closed for replies.

2 replies

Issamos
Super User
September 10, 2023

Hello @mikew67 

I suggest you to install the last version of CubeMX and the last version of your firmware fp-sns-datalog1 (using the firmware installer of CubeMX) and then open the exemple from cube Mx in any IDE you want CubeIDE, keil, IAR).

Best regards.

II

KDJEM.1
ST Technical Moderator
September 11, 2023

Hello @mikew67 ,

After downloading FP-SNS-DATALOG1 repo, could you please import the project "en.fp-sns-datalog1\STM32CubeFunctionPack_DATALOG1_V1.5.0\Projects\STM32L4R9ZI-STWIN\Applications\HSDatalog\STM32CubeIDE" by following the steps in UM2609 - Rev 9 Section 2.10 Importing existing projects.

I hope this help you!

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.