Skip to main content
Associate II
Jan 15, 2026 2:24 AM UTC
Solved

How do i revert the IDE? Version 2.0.0 doesn't have the ability to create a project from a board

I recently upgraded my IDE to version 2.0.  I cannot start a project from the board view; where you select the board type and configure the settings.  It would then create the c++ project code for you.  The new version doesn't have anything to help you select the board and it cannot even open up the board configuration editor when you click on the .ioc file.  Is there. a way to revert back to the previous editor version - I think it was version 1.x.18?

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Jan 15, 2026 7:45 AM UTC

Hello @dshenoy 

In the latest release , STM32CubeMX is no more integrated in STM32CubeIDE 2.0.0 

For more details , please check this STM32CubeIDE 2.0.0 released

 To download CubeMX standalone please use this LINK 

See: STM32CubeIDE 2.0.0 New workflow tutorial

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

TDK
Jan 15, 2026 3:27 AM UTC

Uninstall that version, download the previous version and install it.

STM32CubeIDE | Software - STMicroelectronics

Or use STM32CubeMX in standalone mode as intended.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
Jan 15, 2026 7:45 AM UTC

Hello @dshenoy 

In the latest release , STM32CubeMX is no more integrated in STM32CubeIDE 2.0.0 

For more details , please check this STM32CubeIDE 2.0.0 released

 To download CubeMX standalone please use this LINK 

See: STM32CubeIDE 2.0.0 New workflow tutorial

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.