How do I declare a UART Function in a separate C file?
I have a program that displays the current temperature of a room on the UART terminal and I want to start getting into the habit of separating my functions into their own source and header files, however, I'm running into a couple of problems.
Here is my main header file:
#include "main.h" //Main header file
#include <stdio.h> //Standard header filer
#include <string.h> //String header filer
#include "uart.h"
#define SI7021_ADDRESS_READ (0x40 << 1) | 0x01
#define SI7021_ADDRESS_WRITE (0x40 << 1)
#define SI7021_MEASURE_HUM_NOHOLD 0xF5
#define SI7021_MEASURE_TEMP_NOHOLD 0xF3
char msg[50];
I2C_HandleTypeDef hi2c1;
UART_HandleTypeDef huart2;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2C1_Init(void);
static void MX_USART2_UART_Init(void);
static uint32_t si7021_measure_humidity(I2C_HandleTypeDef *hi2c)
{
uint8_t si7021_buf[4];
si7021_buf[0] = SI7021_MEASURE_HUM_NOHOLD;
// Start measure
int res = HAL_I2C_Master_Transmit(hi2c, SI7021_ADDRESS_WRITE, si7021_buf, 1, 100);
if (res != HAL_OK)
{
return sprintf(msg,"ERROR - Could Not Transmit Humidity\r\n");
uart_send_str (msg);
}
HAL_Delay(30);
// Read result
res = HAL_I2C_Master_Receive(hi2c, SI7021_ADDRESS_READ, si7021_buf, 2, 100);
if (res != HAL_OK)
{
return sprintf(msg,"ERROR - Could Not Receive Humidity\r\n");
uart_send_str (msg);
}
return (si7021_buf[0] << 8 | si7021_buf[1]) * 125 / 65536 - 6;
}
static int32_t si7021_measure_temperature(I2C_HandleTypeDef *hi2c)
{
uint8_t si7021_buf[4];
si7021_buf[0] = SI7021_MEASURE_TEMP_NOHOLD;
// Start measure
int res = HAL_I2C_Master_Transmit(hi2c, SI7021_ADDRESS_WRITE, si7021_buf, 1, 100);
if (res != HAL_OK)
{
return sprintf(msg,"ERROR - Could Not Transmit Humidity\r\n");
uart_send_str (msg);
}
HAL_Delay(30);
// Read result
res = HAL_I2C_Master_Receive(hi2c, SI7021_ADDRESS_READ, si7021_buf, 2, 100);
if (res != HAL_OK)
{
return sprintf(msg,"ERROR - Could Not Receive Humidity\r\n");
uart_send_str (msg);
}
int64_t temp_code = (si7021_buf[0] << 8 | si7021_buf[1]) * 100;
int64_t temp = 17572 * temp_code / 6553500 - 4685;
if (temp > 12500 || temp < -4000)
{
return sprintf(msg,"ERROR - Temperature could not be read properly!\r\n");
uart_send_str (msg);
}
return (int32_t)temp;
}
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_I2C1_Init();
MX_USART2_UART_Init();
while (1)
{
uint32_t humidity = si7021_measure_humidity(&hi2c1);
if (humidity == 0xFFFF){
}
uint32_t temperature = si7021_measure_temperature(&hi2c1);
float temp_C = temperature/100;
sprintf(msg, "%2f C %lu RH\r\n", temp_C, humidity);
uart_send_str (msg);
HAL_Delay(500);
}
}My Uart header file:
#ifndef uart_h
#define uart_h
void uart_send_str (const char* msg);
#endifMy Uart C file:
#include <stdio.h>
#include "uart.h"
#include <stdint.h>
void uart_send_str (const char* msg)
{
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY);
}
I get the following errors:
'huart2' undeclared - first use of this function"
'HAL_MAX_DELAY' undeclared - first use of this function"
Along with an implicit declaration of HAL_UART_Transmit function as a warning.
I know you have to initialize the function before you declare it as typically seen in the main with the "static void MX_USART2_UART_Init(void);" function, but I don't know how to do this in a separate header file.