Skip to main content
JBabl.1
Associate
December 1, 2022
Question

How can I update STM32CubeIDE from version 1.10.1 to version 1.11.0

The "automatic updates" show me a new version 1.11.0. After starting the process it stops with following error:

Problem Occured.

'Updating Sortware' has encounterd a problem. An error occured while collecting items to be intstalled

The details>> shows a large list of errros like this:

An error occurred while collecting items to be installed

session context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).

No repository found containing: osgi.bundle,com.st.stm32cube.common.mx,6.7.0.202211181646

No repository found containing: osgi.bundle,com.st.stm32cube.common.mx.oss,6.7.0.202211181646

No repository found containing: osgi.bundle,com.st.stm32cube.common.mx.stinsider,6.7.0.202211181646

No repository found containing: osgi.bundle,com.st.stm32cube.ide.common.services,2.1.400.202207051747

And so on.

My available software sites under "preferences -> Install/Update" are

0693W00000WJz6QQAT.pngWhat to do to solve this problem?

Please help me.

Thanks Hans

This topic has been closed for replies.

19 replies

JBabl.1
JBabl.1Author
Associate
December 2, 2022

And the next log file

Julien D
ST Employee
December 2, 2022

Interesting!

Given all the No repository found at https://foo.bar exceptions I'm surprised that the Reload had terminated with success.

No repository found at https://sw-center.st.com/stm32cubeide/openstlinux/updatesite1

No repository found at https://sw-center.st.com/stm32cubeide/updatesite1

Those ones are definitely the root cause of the update failure.

The 2 usual causes are :

  1. malformed / corrupted repository
  2. connection issue

1/ is not an option here, I checked it on 2 PCs, 1 being a public computer.

Thus remains the 2/ ..

Are you behind a proxy ? If so, did you well set the proxy settings in STM32CubeIDE (Preferences > General > Network Connections) ? Is it a corporate computer with special IT policies ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JBabl.1
JBabl.1Author
Associate
December 3, 2022

It's really very strange. I'm not behind a proxy and it's my private Laptop at home with no special IT policies.

I also temporarily disabled Norton Security, no effect.

Unitl now i have had no problems with any updates and auto-updates.

The windows control panel for programs shows:

STMicroelectronics STM32CubeIDE 1.8.0 installed on 1.12.2021 2,37GB version 1.8.0

I also have installed STM32CubeProgrammer version 2.9.0 and STMicroelectronics stlink-server version 2.0.2-3

Perhaps this is a help?

S.Ma
Principal
December 5, 2022

Disk space being too low for temp file?

Doing a full separate install instead of upgrades enables incremental debug and backup. Freeware cost you time in this particular case.

Piranha
Principal III
December 5, 2022

It's not because it is free, but because the Eclipse is a junk. It's only slightly better than the HAL broken bloatware and the SalesForce parody of the forum...

EmBitz is also a freeware, but is not a PITA!

Julien D
ST Employee
December 5, 2022

Indeed the disk space could be something to look at, you need at least 2,5Gb.

STM32CubeProgrammer and Stlink-server installations do not interfere with STM32CubeIDE updater.

About your STM32CubeIDE update history, do you remember what was the updated versions starting from 1.8.0 ? All releases (base 1.8.0 -> 1.9.0 -> 1.10.0 -> 1.10.1) ?

Could you also paste screenshots of your current Available Software Sites page and the dialog appearing once the Reload completes ?

If no obvious reason is found you may have to consider what has been already proposed above; do a fresh installation.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JBabl.1
JBabl.1Author
Associate
December 5, 2022

Free disk space could not be the problem: 48,2 Gb.

About the update history: I've done all these steps, for i have checked "Automatically updates"

The screeshot of "Available Software Sites" is on top of this discussion.

The similar dialogs coming now step by step:

JBabl.1
JBabl.1Author
Associate
December 5, 2022

..