Question
How can I setup a project where the ioc file is in a subfolder of the project?
It seems CubeIDE expects the ioc file at the same level as the .project and .cproject are located. When trying to open an ioc which is NOT at the same level as the projects are Iocated, I get this error message: "Invalid Input: Must be project's active .ioc file."
In an existing project we want to upgrade we use 2 ioc configurations. That worked fine until CubeIDE:
[.project]
+-- ASP
+-- HAL_ST
+---- HSE.ioc
+---. HSIStartup
+---- HSI.ioc
I made several tests, trying to add the ioc as link, other places. Open the ioc without a project... Nothing worked.
CubeIDE Version 1.10.1