Skip to main content
YShem.1
Visitor II
February 1, 2020
Question

How can I burn an STM project into the STMF767ZI

1) How can I burn an STM project into the STMF767ZI in the STMCUBEIDE32 after I build the project?

2) The Debug isn't working:

STMicroelectronics ST-LINK GDB server. Version 5.2.3

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

Target unknown error 19

Error in initializing ST-LINK device.

Reason: Unknown. Please check power and cabling to target.

Can somebody guide me how to install the ST-LINK?

I thought I did, I need help step by step please.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
February 1, 2020

A custom board, or a Nucleo?

For the external ST-LINK make sure pin 1/2 have power for the buffers on the pod.

A non-functional chip/board will not be able to connect.

Check connections.

Check level on NRST.

Check power applied to VDDA.

Check voltages/capacitors on VCAP pins.

Do ST-LINK Utilities, or STM32 Cube Programmer find the chip?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..