Skip to main content
KRem.1
Associate
December 8, 2020
Question

Hi, I wanted to use three channel on a single timer. The setup seems to work fine for the first two (ch1 and ch2) but not for ch3. it seems that even with HAL I have to manually set the bit TIM_CCER_CC3E on for ch3. Did I miss something?

I use these fonction to enable all three channels:

HAL_TIM_OnePulse_Start(&htim3, TIM_CHANNEL_1);

HAL_TIM_OnePulse_Start(&htim3, TIM_CHANNEL_2);

 HAL_TIM_OnePulse_Start(&htim3, TIM_CHANNEL_3);

it have to insert this to enable ch3 but just for the channel 3.

htim3.Instance->CCMR2 = TIM_CCMR2_OC3PE| (7<<TIM_CCMR2_OC3M_Pos);

 htim3.Instance->CCER |= TIM_CCER_CC3E

I'm asking this question because I'm not sure if there is an issue with HAL or it's just me.

Best regards,

This topic has been closed for replies.

7 replies

TDK
December 8, 2020

What chip?

"If you feel a post has answered your question, please click ""Accept as Solution""."
KRem.1
KRem.1Author
Associate
December 8, 2020

Stm32f103rb, the nucleo board

TDK
December 8, 2020

TIM_CHANNEL_3 is not a valid argument to HAL_TIM_OnePulse_Start.

https://github.com/STMicroelectronics/STM32CubeF1/blob/003dfc9e6c2e424c19a25df3934afaf7fce660d6/Drivers/STM32F1xx_HAL_Driver/Src/stm32f1xx_hal_tim.c#L2689

/**
 * @brief Starts the TIM One Pulse signal generation.
 * @param htim TIM One Pulse handle
 * @param OutputChannel TIM Channels to be enabled
 * This parameter can be one of the following values:
 * @arg TIM_CHANNEL_1: TIM Channel 1 selected
 * @arg TIM_CHANNEL_2: TIM Channel 2 selected
 * @retval HAL status
 */
HAL_StatusTypeDef HAL_TIM_OnePulse_Start(TIM_HandleTypeDef *htim, uint32_t OutputChannel)

Seems like it should be included, but maybe there's a reason for it being missing.

"If you feel a post has answered your question, please click ""Accept as Solution""."
waclawek.jan
Super User
December 8, 2020

This function (and the related "surroundings" of it) is aimed at one particular application, where one channel serves as a hardware trigger, and the other as output.

 /* Enable the Capture compare and the Input Capture channels

   (in the OPM Mode the two possible channels that can be used are TIM_CHANNEL_1 and TIM_CHANNEL_2)

   if TIM_CHANNEL_1 is used as output, the TIM_CHANNEL_2 will be used as input and

   if TIM_CHANNEL_1 is used as input, the TIM_CHANNEL_2 will be used as output

   in all combinations, the TIM_CHANNEL_1 and TIM_CHANNEL_2 should be enabled together

   No need to enable the counter, it's enabled automatically by hardware

   (the counter starts in response to a stimulus and generate a pulse */

See also the related examples:

Configuration of TIM5 in One Pulse Mode
===================================================
 
 - The external signal is connected to TIM5_CH2 pin (PA.01), 
 and a rising edge on this input is used to trigger the Timer.
 - The One Pulse signal is output on TIM5_CH1 (PA.00).
 
 The delay value is fixed to:
 - Delay = CCR1/TIM5 counter clock 
 = 16383 / 18000000 [sec]
 
 The pulse value is fixed to : 
 - Pulse value = (TIM_Period - TIM_Pulse)/TIM5 counter clock 
 = (65535 - 16383) / 18000000 [sec]
 
 The one pulse waveform can be displayed using an oscilloscope and it looks
 like this.
 
 ____
 | |
 CH2 _________________________| |__________________________________________
 
 ___________________________
 | |
 CH1 ______________________________________| |_____
 <---Delay----><------Pulse--------------->

In other words, this is implementation of a one-shot flip-flop with delay.

This of course is only one very specific application of the OPM in timer. That's Cube/HAL for you.

Oh, and it's an excellent illustration of Cube/HAL documentation, too.

JW

KRem.1
KRem.1Author
Associate
December 8, 2020

ok, thank you.

I may have to adapt this function.

KRem.1
KRem.1Author
Associate
December 13, 2020

Hi,

I finally get my timer working as I wish. I went directly programming the register. In my case, I use the timer 1 to trigger the timer 3 (one pulse mode) on the microcontroler as i needed so extra feature from the timer 1 (the repetition counter).

Apparently, if an internal trigger is selected as the trigger input, it is not needed to configure a channel as an input.

I am a bit concern now, will I still be able to use other hal libraries on my project ?

R.

waclawek.jan
Super User
December 13, 2020

> will I still be able to use other hal libraries on my project ?

Probably yes, if they are not using the given timer(s). I don't use Cube/HAL.

JW