Hi, I just started to use STM32Cube IDE, and I was just workig on a project. I'm using a NUCLEO-F103RB board, but when I build the project (I'm using the default code) there's errors .
The errors are like this one:
In file included from C:/Users/maria/STM32CubeIDE/workspace_1.3.0/led_*****/Drivers/CMSIS/Device/ST/STM32F1xx/Include/stm32f1xx.h:131,
from C:/Users/maria/STM32CubeIDE/workspace_1.3.0/led_*****/Drivers/STM32F1xx_HAL_Driver/Inc/stm32f1xx_hal_def.h:30,
from C:/Users/maria/STM32CubeIDE/workspace_1.3.0/led_*****/Drivers/STM32F1xx_HAL_Driver/Inc/stm32f1xx_hal_rcc.h:29,
from C:/Users/maria/STM32CubeIDE/workspace_1.3.0/led_*****/Core/Inc/stm32f1xx_hal_conf.h:237,
from C:/Users/maria/STM32CubeIDE/workspace_1.3.0/led_*****/Drivers/STM32F1xx_HAL_Driver/Inc/stm32f1xx_hal.h:30,
from ../Drivers/STM32F1xx_HAL_Driver/Src/stm32f1xx_hal.c:36:
C:/Users/maria/STM32CubeIDE/workspace_1.3.0/led_*****/Drivers/CMSIS/Device/ST/STM32F1xx/Include/stm32f103xb.h:132:10: fatal error: core_cm3.h: No such file or directory
132 | #include "core_cm3.h"
| ^~~~~~~~~~~~
compilation terminated.
I'll appreciate the help :)