Skip to main content
Mikey63
Associate
Feb 20, 2020 2:59 PM UTC
Solved

Hello. When I try to install the IDE below I get an error that it is for 64-bit systems only, even though it says x86 in the filename. Is there a suitable V2 IDE on 32-bit for STM32F051? Thanks! Mike. st-stm32cubeide_1.2.0_5034_20200108_0926_x86_64

..

This topic has been closed for replies.

11 replies

Ozone
Principal
Feb 20, 2020 3:08 PM UTC

It does "_64", doesn't it ?

And there are other architectures around, not only x86. Which can be 32 bit or 64 bit.

Usually, 64 bit systems/OSes support 32 bit application versions as well.

Mikey63
Mikey63Author
Associate
Feb 20, 2020 6:59 PM UTC

Well, I would agree with that except I selected the Windows architechture version, so other architectures don't apply. Within windows, if you have a 64-bit system then the x86 folder is where the 32-bit applications go. So an application quoting both is (according to many other developers) compatible with both 32-bit and 64-bit Windows. There are many software programs where you select 64 or x86 versions. It does "x86" doesn't it ? No, it doesn't.

n2wx
Senior
Feb 20, 2020 4:05 PM UTC

If it said i386 then you could expect the 32 bit version. Otherwise what @Ozone​ said.

Piranha
PiranhaBest answer
Principal III
Feb 20, 2020 6:36 PM UTC
Mikey63
Mikey63Author
Associate
Feb 20, 2020 7:27 PM UTC

Thanks Piranha, a helpful response.

n2wx
Senior
Feb 20, 2020 9:31 PM UTC

Buy a new system. There you go.