Skip to main content
NU.2
Associate
June 28, 2020
Question

Hello, I am trying to program STM32F103 MCU barebone. I attached it to LQFP 48 adaptor and made connections to Vcc, GND and clock as in Bluepill module. Using STMCUBE IDE For controlling RGB LED, the code has been debugged and unable to flash.

Error:

Info : clock speed 1800 kHz

Error: init mode failed (unable to connect to the target)

in procedure 'init' 

in procedure 'ocd_bouncer'

I set high freq clock as ceramic resonator (used 8Mhz clock chipset) and with STLINK V2 debugger.

Please let me know the issue i am encountering. Thanks for your time:)

This topic has been closed for replies.

3 replies

mattias norlander
ST Technical Moderator
June 30, 2020

We probably need more info about which pins of the F103 that you have connected which pins of the ST-LINK V2. Can you post a table of this? Vcc, Gnd and Clk is not enough. Assuming SWD, how about SWDIO? NRST?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
LaurentL
ST Employee
June 30, 2020

Hi,

If you don't connect the reset line from the STLink, you have to avoid using the "connect under reset" strategy.

Try with reset none in debugger tab in debug config.

Or add the Reset connection and try without changing anything else.

Rgds,

Laurent

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
NU.2
NU.2Author
Associate
June 30, 2020

Thanks!

I encountered couple of issues and it's finally ok now.

​>> First if all, my workspace had special characters in name (projects & design) and the software took it as "projects&". Got it fixed after changing this.

​

>> I wiped the MCU flash using STLink utility and programming it worked then on.

​

>> The MCU came with Blinky LED program and when I was trying to program, it got interference and failed to load. Attaching a reset switch and holding it for 5 seconds before uploading code worked.

​

Perfect!