Skip to main content
LGuo
Associate
July 22, 2019
Question

Has anyone seen for compiling error for dspin.h for not having the valid preprocessing token? How to resolve it?

​In dspin.h file

#define CHECK_REG(reg, result) if (dSPIN_RegsStruct-> ## reg != dSPIN_Get_Param(dSPIN_ ## reg)) result |= 1 << ((uint8_t) dSPIN_ ## reg)

Compiling error for dspin.c

uint32_t dSPIN_Registers_Check(dSPIN_RegsStruct_TypeDef* dSPIN_RegsStruct)

{

uint32_t result = 0;

CHECK_REG(ABS_POS, result);

make -j8 all

arm-none-eabi-gcc "../Src/dspin.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Src/dspin.d" -MT"Src/dspin.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Src/dspin.o"

arm-none-eabi-gcc "../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc.d" -MT"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc.o"

arm-none-eabi-gcc "../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc_ex.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc_ex.d" -MT"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc_ex.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_rcc_ex.o"

arm-none-eabi-gcc "../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.d" -MT"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.o"

arm-none-eabi-gcc "../Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim_ex.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32F767xx -DDEBUG -c -I../Inc -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32F7xx/Include -I../Drivers/STM32F7xx_HAL_Driver/Inc -I../Drivers/STM32F7xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim_ex.d" -MT"Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim_ex.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim_ex.o"

In file included from ../Inc/dspin_config.h:27:0,

from ../Src/dspin.c:24:

../Src/dspin.c: In function 'dSPIN_Registers_Get':

../Inc/dspin.h:889:35: error: pasting "->" and "ABS_POS" does not give a valid preprocessing token

if (read_reg != dSPIN_RegsStruct-> ## reg_name) strcpy(diff,"x"); \

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
July 22, 2019

So grep project and see what ABS_POS is set to, and if you have missing or multiple instances of it.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LGuo
LGuoAuthor
Associate
July 22, 2019

​Hi Clive,

Thanks for your reply. It looks like the compiler is not able to recognize the Macro token paste operator : ##. The compiler supposedly should be able to preprocess the macro CHECK_REF(ABS_POS, result) by replacing it with if (dSPIN_RegsStruct-> ABS_POS != dSPIN_Get_Param(dSPIN_ ABS_POS)) result |= 1 << ((uint8_t) dSPIN_ ABS_POS

Is there any option in the compiler I need to turn so that the compiler is able to support the Token Paste Operator : ##?

Thanks a lot.

Tesla DeLorean
Guru
July 22, 2019

Sounds more like it is working but one or more of the things it is trying to paste together is wrong.

Do any of the demo projects using dspin.c work/build properly?

Can you enable the compiler to output the pre-processor pass of the source so you can inspect/review that?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
LGuo
LGuoAuthor
Associate
July 22, 2019

​Do you know how? It seems I was not able to find such a compiler option setting. Thanks