Skip to main content
Associate III
April 3, 2024
Question

Hardfault handler infinite loop

Hello,

 

I am currently using a Nucleo F446RE board and i am facing problem while trying to read an analog pin using ADC functions. When i start running or debugging the project, i immediately fall down into Hardfault_handler function. I don't know what i exactly did wrong, and don't know how to figure it out...

 

Thanks in advance for help!

 

Please find attached the main file i wrote.

    This topic has been closed for replies.

    5 replies

    mƎALLEm
    ST Technical Moderator
    April 3, 2024

    Hello,

    At a first glance you declared this table with one element:

    uint16_t uiADCRawValueBuffer[1];

      Then you access two elements.

    uint16_t uiADCRawValueBuffer[1];
    
    		for (int var = 0; var < 2; ++var) {
    			uiADCRawValueBuffer[var] = HAL_ADC_GetValue(&hadc1); // Store converted values
    		}
    		buffer_throttle = uiADCRawValueBuffer[0];
    		buffer_brake = uiADCRawValueBuffer[1];

      Please check.

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
    Erwan03Author
    Associate III
    April 3, 2024

    Hello SofLit! hope you're doing well!

    Ok then i changed 

    uint16_t uiADCRawValueBuffer[1];

    to

    uint16_t uiADCRawValueBuffer[2];

    so i have enough element in this array. But i am still stuck with same problem. Cannot debug nor Run. 

    Let's start with only 1 analog input. Throttle one.

    mƎALLEm
    ST Technical Moderator
    April 3, 2024

    Not obvious to find the problem with the info you provide.

    This kind of issue needs a debug. So go step by step and find at which step you get the hardfault. 

    You can comment out the code and uncomment line by line and find at which level the hardfault occurs.

    To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.