Skip to main content
Associate III
August 22, 2023
Question

HAL_I2C_Mem_Write Stuck

Hi everyone,

 

i am working on a STM32C011F6P6

i am trying to apply some I2C setting to other chip

normal writing value to corresponding address
but seems the HAL_I2C_Mem_Write function is stucked

these are the read and write function

HAL_StatusTypeDef i2c_write_reg(uint8_t reg, uint8_t send_data ) {
 	return HAL_I2C_Mem_Write(&hi2c1, SLAVE_ADDRESS<<1 , reg, I2C_MEMADD_SIZE_8BIT ,&send_data, 1 , HAL_MAX_DELAY);

}

uint8_t i2c_read_reg(uint8_t reg) {
 uint8_t temp;

 if (HAL_I2C_Mem_Read(&hi2c1, SLAVE_ADDRESS << 1, reg, I2C_MEMADD_SIZE_8BIT, &temp, 1, HAL_MAX_DELAY) != HAL_OK) {
 // Handle error here
 return 0; // Or any default value you prefer
 }

 return temp; // Success, return the read value
}

 these are the code execute

HAL_StatusTypeDef stat2;
	stat2 = i2c_write_reg(0x25,0x70);
	if(stat2!=HAL_OK){
		printf("HAL not ok\r\n");
	}
	stat2 =i2c_write_reg(0x26,0x07);
	if(stat2!=HAL_OK){
		printf("HAL not ok\r\n");
	}

	uint8_t x ;

	x = i2c_read_reg(0x25) ;
	printf("0x250x%02x\r\n",x);
	x = i2c_read_reg(0x26) ;
	printf("0x26:0x%02x\r\n",x);



i already have pull up resistor on board

any solution or any thing i can do to identify the real issue?

    This topic has been closed for replies.

    6 replies

    RhSilicon
    Lead
    August 22, 2023

    any solution or any thing i can do to identify the real issue?

    I don't know if it can help in your case, but I found these videos about advanced debugging:

    STM32CubeIDE Advanced Debug Features
    https://youtube.com/playlist?list=PLnMKNibPkDnEDEsV7IBXNvg7oNn3MfRd6

    TDK
    August 22, 2023

    Always use HAL_I2C_IsDeviceReady first to verify the device is responding before using other functions.

    My guess is the bus is stuck to due debugging/previous activity on bus. In which case you need to toggle SCL 9 times at startup before initializing it as I2C. Or power cycle everything.

    If HAL_I2C_IsDeviceReady does not pass for this chip, then problem could be somewhere else.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    Associate III
    August 23, 2023

    just found is my slave device have not powered at the first place

    now it can return hal_err

    thinking why it is not working

    TDK
    August 23, 2023

    If your slave device is not powered, it's not likely to respond to commands. It will also generally pull the SDA and SCL lines down and prevent you from using them effectively.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    Foued_KH
    ST Employee
    August 23, 2023

    Hello @uveuvenouve , 

    I suggest you use an oscilloscope to check SDA and SCL behavior or try to debug and set breakpoints .

    Foued

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    Associate III
    August 24, 2023

    just found i may have messed up the slave id setting
    i thought setting slave id in i2c mean the target slave device

    but seems that is stating own slave id
    and i have 2 devices connected to the target slave device
    so i think they some how conflicted by falsely setting all 3 devices have same slave id