Skip to main content
Associate II
Aug 8, 2025 7:34 AM UTC
Solved

H503RB, USBX, ThreadX: Thread blocked by USBX

Hello,

I have an issue with this setup:

  • STM32H503RB
  • CubeIDE 1.19.0, Win10
  • ioc-Implementations:
    SYS[Timebase Source TIM1]; RCC[CRS SYNC Source USB]; ICACHE[1way]
    Connectivity-> USB[Device only, USB FS Global Interrupt, Internal PHY]; SPI3[FD-Master]
    Middleware-> TREADX[Core]; USBX[Core, Device CoreStack FS, Device Controllers FS, CDC ACM]

Nothing is implemented regarding the SPI port yet.
I succesfully went through this STM tutorial: https://www.youtube.com/watch?v=LdY2bieaPwk 

Success means: when I switch the PC13 button, the string "Hello World" is transmitted to the terminal on my PC.

Here is the But:
A thread for the blinking of an LED is not running anymore:

VOID LD1_thread_entry(ULONG initial_input){
	(VOID)initial_input;
	while(1){
		HAL_GPIO_TogglePin(LED_RD1_o_GPIO_Port,LED_RD1_o_Pin);
		tx_thread_sleep(8); // 1tick per 10ms
	}
}

I know the workaround already:

  • Priority of usbx-write-thread is [Prio,Subprio=] 9,9
  • Priority of LD1_thread is 15,15
    => just decrease from 15,15 to lower values and it works. With values of 9,9 or lower the LED is blinking.

But my understanding is lacking here:
The usbx process is just this:

VOID usbx_cdc_acm_write_thread_entry(ULONG thread_input)
{
	UX_PARAMETER_NOT_USED(thread_input);
	ULONG actual_length;
	while(1)
	{
		// wait for button press
		tx_semaphore_get(&semaphore, TX_WAIT_FOREVER);

		// transmit data
		ux_device_class_cdc_acm_write(cdc_acm, (UCHAR *)(&Tx_Buffer), (strlen(Tx_Buffer)), &actual_length);
	}
}

So all the time while I am not pressing the button, usbx_write_thread is just waiting for the semaphore. By definition is "sleeping" until semaphore wakes the thread up.

But how can this sleeping-process prevent a (low priority) task (LED blinking) from being executed?
The concept of ThreadX is that exactly this should never happen.

I would be grateful if someone knows where "the bug" is.

In case you need more information about the background/code/... just let me know. Right now my code really looks like in the tutorial plus the LED stuff.
Thanks in advance!
Enrico

This topic has been closed for replies.
enbwBest answer
Associate II
Aug 12, 2025 2:12 PM UTC

Bug was fixed:
the issue was a while(1) loop. In the tutorial this while(1); was suggested in the function app_ux_device_thread_entry() in app_usbx_device.c by the tutorial. But it blocks the other (low priority) tasks from being executed.

This function is just for configuration so, the while(1) can simply be deleted.

1 reply

enbwAuthorBest answer
Associate II
Aug 12, 2025 2:12 PM UTC

Bug was fixed:
the issue was a while(1) loop. In the tutorial this while(1); was suggested in the function app_ux_device_thread_entry() in app_usbx_device.c by the tutorial. But it blocks the other (low priority) tasks from being executed.

This function is just for configuration so, the while(1) can simply be deleted.