Skip to main content
ggowd.1
Associate III
October 18, 2024
Question

Generating code for HTTPD in NUCLEO-H745ZI Board

Hi Team,

"I am trying to configure an HTTP server on the Nucleo-H745ZIT6 board, which has two Cortex cores. I am using Cortex-M7 for this. After enabling HTTP in middleware inside LwIP, and generating the code, LwIP is placed inside the Cortex-M7 folder, but the HTTP code is generated outside of it. When compiling, I get an error saying 'fsdata.c: No such directory.' They are adding the HTTP image inside the HTTP folder, but I need to configure the resources configuration but not getting the option and I'm not sure how. Can you help me with this?"

i am using stmcubeide 1.15.1 software

Best Regards,
Gagan Gowda

This topic has been closed for replies.

5 replies

Ghofrane GSOURI
ST Technical Moderator
October 18, 2024

Hello @ggowd.1 

First I recommend you  to use the latest version of CubeMX 6.12.1 and CubeIDE 1.16.1 

After checking your IOC , all you need to do is to add the fsdata.c manually  to your project ,

If "fsdata.c" has not been copied in your project, it can be taken from the Firmware Repository (Menu Help > Updater Settings...) Software Package folder within Middlewares\Third_Party\LwIP\src\apps\http folder.

actually those informations  are mentioned in parameter description 

GhofraneGSOURI_0-1729251389977.png

GhofraneGSOURI_1-1729251455307.png

GhofraneGSOURI_2-1729251872285.png

 

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ggowd.1
ggowd.1Author
Associate III
October 18, 2024

Hi @Ghofrane GSOURI 

I added fsdata.c and fsdata_custom.c to the HTTP folder. After that, when I called httpd_init(), I received a warning: 'implicit declaration of function httpd_init'. What should I do to resolve this?"

PFA of http folder i am not arrow of that folder

Best Regards,
Gagan Gowda

Ghofrane GSOURI
ST Technical Moderator
October 18, 2024

The warning "implicit declaration of function ''httpd_init'' indicates that the compiler encountered a call to the "httpd_init" function before it had seen a declaration or definition for that function.

httpd_init function is declared in httpd.c file and you want to use it in fs.c file  ,just Include this header in your fs.c file:

#include "lwip/apps/httpd.h"

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.