From TrueStudio to STM32CubeIDE how to?
- 2 replies
- 1048 views
Until now I used TrueStudio.
But now I generated a project for STM32CubeIDE, suing the seprated CubeMX.
I'm using STM32CubeIDE Version 1.3.0, STMCuneMX Version 5.6.1
Reinstalled both, but no luck to get it working on Windows 10.
And get these error when compiling:
...
specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Src/wwdg.o"
USBD_StatusTypeDef USBD_LL_Transmit(USBD_HandleTypeDef *pdev, uint8_t ep_addr, uint8_t *pbuf, uint32_t size)
^~~~~~~~~~~~~~~~
In file included from ../Src/usbd_conf.c:26:0:
../Middlewares/ST/STM32_USB_Device_Library/Core/Inc/usbd_core.h:127:21: note: previous declaration of 'USBD_LL_Transmit' was here
USBD_StatusTypeDef USBD_LL_Transmit (USBD_HandleTypeDef *pdev,
^~~~~~~~~~~~~~~~
../Src/usbd_conf.c:592:20: error: conflicting types for 'USBD_LL_PrepareReceive'
USBD_StatusTypeDef USBD_LL_PrepareReceive(USBD_HandleTypeDef *pdev, uint8_t ep_addr, uint8_t *pbuf, uint32_t size)
^~~~~~~~~~~~~~~~~~~~~~
In file included from ../Src/usbd_conf.c:26:0:
../Middlewares/ST/STM32_USB_Device_Library/Core/Inc/usbd_core.h:132:21: note: previous declaration of 'USBD_LL_PrepareReceive' was here
USBD_StatusTypeDef USBD_LL_PrepareReceive(USBD_HandleTypeDef *pdev,
^~~~~~~~~~~~~~~~~~~~~~
make: *** [Src/subdir.mk:134: Src/usbd_conf.o] Error 1
make: *** Waiting for unfinished jobs....
"make -j8 all" terminated with exit code 2. Build might be incomplete.
Has anybody seen this?
I will try with the inmtegrated CubeMX now...
Update: ioc files from other STM32CubeMX versions cause these problems.
While they seem to look right in STM32CubeMX , under the hood things seem to go wrong.
Just needed to redo everything, generating a new ioc.