Skip to main content
Benjamin Brammer
Senior II
February 24, 2020
Question

FreeRTOS and SEGGER SystemView not working

Hello,

I am trying to get FreeRTOS and SEGGER SystemView (3.1) to run on an STM32F103RCTx. I used the appropriate manual from SEGGER to include all the necessary folders in my project. Although I have included all the new folders in the Include Paths I get the following error when compyling:

0690X00000DCBtNQAX.png

When searching for help with google, I often read that I have to update the Linker to see this new folder as a library. When I do so in the C/C++ settings I get the following error:

0690X00000DCBv0QAH.png

does anybody know what I am doing wrong and how I can fix this problem?

Benjamin

This topic has been closed for replies.

1 reply

Giulio Dalla Vecchia
Associate II
March 12, 2020

Hello Benjamin,

I have the same problem! But if you have a look well in file "SEGGER_SYSVIEW_Conf.h", no one preprocessor macros are defined probably. So, in my case there aren't any __ARM_ARCH_'V'__ defined. (I'm working with a STM32F302CB with STM32CubeIDE)

I hope some ST Member can help us to solve the problem.

GDV