Skip to main content
Associate III
Apr 2, 2026 12:34 PM UTC
Solved

Floating Point variable debug - limit decimal places ?

To sum up my project, i get temperature value from NTC. I made ADC reading. There is no problem about getting values. I define temperature value as floating point variable. When observing it on debug screen, because it was floating, numbers after . is too much like seven digit. As you see in picture, is there any way to reduce the number of digits on debug window?

 

temperatureDisplaytemperatureDisplay

 

Andrew Neil
Andrew NeilBest answer
Super User
Apr 2, 2026 2:15 PM UTC

@Ozone wrote:

Not using float at all will save you several kB of code space.


Indeed.

Even though the F4 does have an FPU, it is only single-precision - which can cause issues with standard C libraries:

Be aware: Floating Point Operations on ARM Cortex-M4F

 

And that's apart from all the other issues inherent in floating-point on binary computers:

Pitfalls of Floating-Point Numbers (And How To Avoid Them)

What every computer scientist should know about floating-point arithmetic

See also: https://docs.oracle.com/cd/E19957-01/806-3568/ncg_goldberg.html 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

9 replies

Andrew Neil
Super User
Apr 2, 2026 12:45 PM UTC

@tensaisakuragi06 wrote:

I define temperature value as floating point variable.


Why ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate III
Apr 2, 2026 12:48 PM UTC

Its a little disturbing. It feels like value changes frequently. I do not need precise measurement. Just two digits is enough for me. This is actually not a problem. I seek for if it was possible.

Ozone
Principal
Apr 2, 2026 1:18 PM UTC

You can do the calculation in integer. Or in integer fractions ("scaled math", e.g. in 1/10th °C).
Not using float at all will save you several kB of code space.

I can't really comment on the CubeIDE debugger, I don't use it.
But I would check if the context menu has such a precision option, or check the manual.

Andrew Neil
Andrew NeilBest answer
Super User
Apr 2, 2026 2:15 PM UTC

@Ozone wrote:

Not using float at all will save you several kB of code space.


Indeed.

Even though the F4 does have an FPU, it is only single-precision - which can cause issues with standard C libraries:

Be aware: Floating Point Operations on ARM Cortex-M4F

 

And that's apart from all the other issues inherent in floating-point on binary computers:

Pitfalls of Floating-Point Numbers (And How To Avoid Them)

What every computer scientist should know about floating-point arithmetic

See also: https://docs.oracle.com/cd/E19957-01/806-3568/ncg_goldberg.html 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
waclawek.jan
Super User
Apr 2, 2026 1:17 PM UTC

Instead of the variable itself, you can perhaps display an expression which contains rounded/truncated value.

Just an idea to be experimented with, maybe not viable - I don't use Cube.

JW

Associate III
Apr 2, 2026 1:22 PM UTC

In excell, it gives option show two digits after , :) . Its not a major problem(it is actually not a problem). Maybe later this option can be added. I am not sure this kind of thing is logical or not. By the way, when i display value on LCD or OLED(any kind of screen), i can display it as two digits after . as library functions allows me to do. So, if it is not possible i can left it as it is.

unsigned_char_array
Lead III
Apr 2, 2026 2:32 PM UTC

You may want to scale to an integer. If you want 2 digits multiply by 100, if you want 3 multiply by 1000. etc. Add 0.5 to round.

 
Screenshot 2026-04-02 162645.png

You can also scale back to float/double, but the downside is that you cannot represent all decimal fractions perfectly with powers of 2. Such as 0.1:

Screenshot 2026-04-02 163046.png

If you want more options you can use snprintf to print the value to a string and then add the string to live expression.

 

 

Screenshot 2026-04-02 163706.png

Screenshot 2026-04-02 164008.png

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."