Skip to main content
Associate II
February 8, 2024
Solved

Flash binaries in STM32F7

Hi all,

I have a project on a STM32F7 target and I work on STM32CubeIDE.
How can I generate the binaries from the code ? And how can I flash the binaries in the STM32F7 (in NUCLEO-STM32F7ZG board) ?
I don't want to use the "flash" button of the app, as if I was a client with only binaries of the code.

Thank you for your help.
Best regards

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    February 8, 2024

    @Remi99 The STM32CubeIDE also generates BIN files directly if you tick Convert to binary file in:

    Project > Properties > C/C++ Build > Settings > MCU Post build outputs

    NUCLEO boards like yours do not necessarily need a dedicated programming software because the embedded ST-LINK/V2-1 is visible as a mass storage device when connected to the PC via USB. The BIN can then be copied there using the normal copy command of the operating system, the ST-LINK/V2-1 then takes over the programming of the target.

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    3 replies

    TDK
    February 8, 2024

    Use STM32CubeProgrammer to flash a binary file (ELF, HEX, or BIN). When you compile code in STM32CubeIDE, this file is produces and put into the Debug/ or Release/ directory within the project.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    Tesla DeLorean
    Guru
    February 8, 2024

    OBJCOPY should be able to generate .BIN files from .ELF,  FROMELF too

    Host of other applications capable of converting HEX to BIN

    Programming NUCLEO board, just use STM32 Cube Programmer. ST-LINK Utilities should also be fine with ST-LINK/V2 and F7 devices.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    February 8, 2024

    @Remi99 The STM32CubeIDE also generates BIN files directly if you tick Convert to binary file in:

    Project > Properties > C/C++ Build > Settings > MCU Post build outputs

    NUCLEO boards like yours do not necessarily need a dedicated programming software because the embedded ST-LINK/V2-1 is visible as a mass storage device when connected to the PC via USB. The BIN can then be copied there using the normal copy command of the operating system, the ST-LINK/V2-1 then takes over the programming of the target.

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.