Skip to main content
Markus GIRDLAND
ST Employee
May 15, 2019
Question

Features and known issues in STM32CubeIDE

Dear community,

Edit: This thread was initially made to clear up some confusion about what functionality STM32CubeIDE was intended to have. As the tool has now been released for a while I believe that is has become more clear. However, having easy access to the known problems and limitations is still very helpful so I will keep this thread pinned.

Although, to spare myself from having to continuously update this thread I will simply link to the release note where this information is available:

The release note can be found here (RN0114).

This topic has been closed for replies.

41 replies

BCoch
Senior
May 21, 2019

Thanks for posting this. Any insight into which of these issues are being worked on, and/or roughly when the next release might be available?

Markus GIRDLAND
ST Employee
May 22, 2019

I don't want to speculate as deadlines and content of a release can rapidly change in software development.

Even if I guessed a rough estimation it might set expectations of a release that we later can't fulfill.

Once I know with more certainty I might be able to share details.

Michael B
Associate III
September 25, 2019

Do we have any idea yet on when a version update will be released? It's been a long time, is your release cycle really that long? There are so many bugs in the IDE especially relating to TouchGFX and CubeMX code generation, XML cproject generation and also with debugging.

shorai
Associate III
June 5, 2019

Here's my 2c.

Overall a step (several steps!) in the correct direction, well done.

TouchGFX downloads a windows msi package that will not install on Linux.

I tried to use the 'Graphics simulator' on a STM32F429ZI Disco and that doesn't work - none of the pins are assigned let alone imports of the libraries. OK, I see TouchGFX is still being integrated and there are problems on the 746 as well. The middleware item 'Graphics' is greyed out but is active. The dropdown to select 'Graphics Framework' and 'Graphics Display' are similarly greyed out but inactive.

As a result one never knows what the colours on the IDE mean and the user is always confused. The greyed 'graphics' texts above are inactive, others are inactive, a grey cancel button is active! Text colouring should obey de facto standards and never be confusing. The graphics department need to understand the day to day needs of technical users.

Consistent icons, colours and shading are vital in order to get IDEs accepted. Grey should be reserved for 'Inactive' as with almost all GUI applications (it was a Windows, XServer and IBM GUI standard some years back, ). The graphic designers are wrong, it is misleading, more difficult to read, ambiguous and error prone. Software developers have sufficient other problems not to need to add poor graphics to them.

Grey text on white and vice-versa is difficult to read in certain light conditions, as is light yellow (or any other colour) on white or cream. Bring the contrast to usable levels.

Can we get right button and mouse over explanatory text? Where do I get documentation on what 'Graphics Simulator' means? (Right Click ->Help????)

Come to think of it, help should be available from anywhere ... right down to Reference manual RMxxxxx level.

I would also, in some cases, just want the old BSP graphics, TS drivers, Buttons, I2C peripherals - nowhere to be found other than digging and copying them deep in the file system.

The 'Additional Software' items need more than just a short description hidden at the right hand side. Clickable documentation links would help, Mouse over balloons would be better.

Rather give single option defaulted to the current release (it is a new project isnt't it?) than all versions. Use the screen space freed to provide a better description of the library (LS3xx Accellerometer and Gyro is better than MEMS, which could be anything). I need at this time to know what the device DOES and not its technology.

The old cube did not seem to remember that I was working with a board level product. The new one does not even give me the option to 'set all peripherals to default values' and include the necessary drivers.

The IDE should be extended to provide a board level view as well as the chip level view. Something like the Open MBED colour coded cards would be SO nice to have in the IDE.

It is interesting to note that nearly all the above comments do not require great changes and development of the code base, they require the presentation team to creatively use and present the features already available.

Am I the only one with this perspective?

Adam Hamilton
Senior
June 21, 2019

Yes, I think the same.

Is there a bug tracker for the STM32CubeIDE.

If not, there should be one where one can file bugs and vote on ones the community believes to be of high importance.

GStap
Associate
June 21, 2019

I agree. I don't know if Github allows voting, but otherwise it would be a great place to report and track bugs, if someone from ST is willing to set up a project page. This could also be a great place to start making both an official ST, and community, wiki to support ST products. ST employees/engineers should be able to easily update a public-facing wiki, and customers should have access to a parallel wiki to arbitrarily add useful content as well.

Michael98006
Associate III
June 25, 2019

There seems to be a bug that causes you to lose your files. I'm running version 1.0.1 of CubeIDE (build 3139_20190612-1256). When I tried to create a new project in my C:\Projects folder, I thought the IDE would create a new folder inside C:\Projects based on the project name I gave it. Instead, it erased all my files and folders in C:\Projects and errored out creating my project directly in C:\Projects. There should have been a warning explaining where the new project would be created. And no files should have been deleted in the target folder.

BCoch
Senior
June 25, 2019

I've also run into the problem where it unexpectedly creates the files directly in the top level directory, (then takes forever to complete if there are already a lot of other files or projects there). I don't think it deleted anything though. I think it does give a warning if the directory doesn't exist - which is probably the desired, normal case.

Markus GIRDLAND
ST Employee
June 26, 2019

There's a ticket and I've seen some reports about possible deletion of code upon problems with project regeneration. But you guys ran into this problem upon project creation? If so, do you have a reliable way to recreate it?

BCoch
Senior
June 25, 2019

I prefer to use only LL drivers, so the bug where it adds HAL back in anytime anything is changed is the most annoying bug to me. (It does this even if you're careful to ensure only LL drivers are specified before generating code.) The only way I've found to fix it is to directly edit the .cproject and .mxproject files.

matheusmbar
Associate
July 1, 2019

I've been running STM32CubeIDE in the last weeks in MacOS and Linux and there is no auto complete suggestions working whatsoever

Everything was working correctly in TrueStudio in this project that I've imported to STM32Cube IDE.

Is there some required configuration to execute? Any work around ?

EDIT:

Just found a fix for that in this post: https://community.st.com/s/question/0D50X0000AkRr8fSQC/stm32cubeide-autocomplete-ctrlspace-is-not-working

There is a config required to enable the auto complete correctly

IPetl
Visitor II
July 6, 2019

Hi.

In my project I use some partions of conditionally compiled code accordingly to Cortex-M0 or Cortex-M3/4 core selected. Code compiles fine, but there is issue with Eclipse Indexer.

MCU ARM GCC Built-in Compiler Settings provider shows such ARM architecture version which should be 6 or 7 instead:

After some investigation I found that for some reason ${FLAGS} not substituted during compiler properties scanner invoking, so it returns default architecture i think.

Default scanner invoking string (not changed):

${COMMAND} ${FLAGS} -E -P -v -dD "${INPUTS}"

Which leads to such log in console:

12:47:10 **** Running scanner discovery: MCU ARM GCC Built-in Compiler Settings ****
arm-none-eabi-g++ -E -P -v -dD C:/......

If I will manually change scanner invoking string to:

${COMMAND} ${FLAGS} -mcpu=cortex-m4 -std=gnu11 -E -P -v -dD "${INPUTS}"

I will get correct scanner result for ARM architecture:

12:47:10 **** Running scanner discovery: MCU ARM GCC Built-in Compiler Settings ****
arm-none-eabi-g++ -mcpu=cortex-m4 -std=gnu11 -E -P -v -dD C:/......

Eclipse Indexer is powerfull feature, however this bug leads to incorrect indexing result and code highlight accordingly to compiler's built-in macro definitions. Will it be fixed in future?

themole
Associate II
July 16, 2019

SFRs View is missing register descriptions, because the column is missing and it is not possible to add it simply. The description shows up in the details view:

0690X000009YoQcQAK.png

mattias norlander
ST Employee
September 5, 2019

Well this is intended. The SFR-view shows more detailed information (stored in the svd-file) in the bottom instead of occupying horizontal space with a bunch of columns.

BCoch
Senior
August 5, 2019

One feature that would be helpful would be the ability to change devices without starting from scratch. For example at least being able to switch between different pin count versions of the same part. This would help with switching from a Nucleo or Discovery board to a custom board.

TLeaf
Associate
August 6, 2019

Maybe another defect for 1.0.2.

After upgrading to 1.0.2, every time I click the 'generate code' button, my C++ project will be converted to C project, and I have to covert it back manually.

This problem was not exist in verion 1.0.1.