Skip to main content
Associate
August 31, 2023
Solved

FDCAN setup on Riverdi display STM32H757XIH6

Hi everyone,

I bought a display Riverdi display (RVT70HSSNWC00-B) with a STM32H757XIH6 microcontroller.

I want to setup the FDCAN but without success.

Has anybody already done and could send a sample ?

Thank you in advance.

This topic has been closed for replies.
Souhaib MAZHOUDBest answer
ST Technical Moderator
August 31, 2023

Hi @AlexandreTe 

Thank you for posting!.

You can check out this video FDCAN Normal Operating Mode - YouTube  for an exemple of FDCAN configuration with STM32H7.  

And i advise to refer this document Introduction to FDCAN peripherals for STM32 product classes - Application note, it will give you an overview of FDCAN peripherals for STM32.

Thank you.

Souhaib

 

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

10 replies

Souhaib MAZHOUDBest answer
ST Technical Moderator
August 31, 2023

Hi @AlexandreTe 

Thank you for posting!.

You can check out this video FDCAN Normal Operating Mode - YouTube  for an exemple of FDCAN configuration with STM32H7.  

And i advise to refer this document Introduction to FDCAN peripherals for STM32 product classes - Application note, it will give you an overview of FDCAN peripherals for STM32.

Thank you.

Souhaib

 

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate
September 4, 2023

Hi Souhaib,

Thank you for your reply.

I watch the video you have sent,after that sending message works but receive not works.

Have you got a project which works with the riverdi product ?

 

Thank you.

 

Alexandre

Issamos
Super User
September 4, 2023

Hello @AlexandreTe 

I think this two articles could help you (with video demonstration).

Hope this is helpful for you. If your question is answered please check this answer as best answer to be diffused.

Best regards.

II

Associate
September 5, 2023

Hi Issamos,

Thank you for your reply.

Finally, I find what to change using the code provide by ST. It is just a little bit different using touchgfx.

I close this subject.

Associate
May 25, 2024

Hi, I have the same problem with fdcan, I send it but I can't receive anything. Can you tell me what needs to be changed in the code? I use riverdi lcd with stm32 board.

Many Thanks

Associate III
October 24, 2023

Hi all,

I want to know if I have to supply FD CAN transciever in order to work correctly with it.

Thank you again.

Associate
May 28, 2024

Hi,

Here is my notes for a project test, I hope this will help you :

fdcan.c

/* USER CODE END FDCAN1_Init 1 */
 hfdcan1.Instance = FDCAN1;
 hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
 hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
 hfdcan1.Init.AutoRetransmission = DISABLE;
 hfdcan1.Init.TransmitPause = DISABLE;
 hfdcan1.Init.ProtocolException = DISABLE;
 hfdcan1.Init.NominalPrescaler = 16;
 hfdcan1.Init.NominalSyncJumpWidth = 1;
 hfdcan1.Init.NominalTimeSeg1 = 2;
 hfdcan1.Init.NominalTimeSeg2 = 2;
 hfdcan1.Init.DataPrescaler = 1;
 hfdcan1.Init.DataSyncJumpWidth = 1;
 hfdcan1.Init.DataTimeSeg1 = 1;
 hfdcan1.Init.DataTimeSeg2 = 1;
 hfdcan1.Init.MessageRAMOffset = 0;
 hfdcan1.Init.StdFiltersNbr = 2; //un filtre par trame entrante
 hfdcan1.Init.ExtFiltersNbr = 0;
 hfdcan1.Init.RxFifo0ElmtsNbr = 0;
 hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
 hfdcan1.Init.RxFifo1ElmtsNbr = 0;
 hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
 hfdcan1.Init.RxBuffersNbr = 2; //un buffer par trame entrante
 hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_12; //8
 hfdcan1.Init.TxEventsNbr = 0;
 hfdcan1.Init.TxBuffersNbr = 2; //un buffer par trame sortante
 hfdcan1.Init.TxFifoQueueElmtsNbr = 0;
 hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
 hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_12; //8
 if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN FDCAN1_Init 2 */

main.c

/* USER CODE BEGIN PV */
FDCAN_FilterTypeDef sFilterConfig; //filtre de la première trame
FDCAN_TxHeaderTypeDef TxHeader; //Première trame sortante
FDCAN_RxHeaderTypeDef RxHeader; //Première trame entrante
uint8_t TxData_Node1_To_Node2[8]={0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0}; //data première trame sortante
uint8_t RxData_From_Node2[12]; //data première trame entrante

FDCAN_FilterTypeDef sFilterConfig2; //filtre de la deuxième trame
FDCAN_TxHeaderTypeDef TxHeader2; //deuxième trame sortante
FDCAN_RxHeaderTypeDef RxHeader2; //deuxième trame entrante
uint8_t TxData_Node1_To_Node22[8]={0x0,0x0,0x0,0x0,0x0,0x0,0x0,0x0}; //data deuxième trame sortante
uint8_t RxData_From_Node22[12]; //data deuxième trame sortante
/* USER CODE END PV */

 /* USER CODE BEGIN 2 */


 if (BSP_SDRAM_SingleTest() != 0)
 {
	 // Error_Handler();
 }


 if (CSP_QUADSPI_Init() == HAL_OK) {
	 CSP_QSPI_EnableMemoryMappedMode();
 }



 // DEMO_RibusDisplayQuery( );

 if (HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_1) != HAL_OK)
 {
 /* PWM Generation Error */
 Error_Handler();
 }

//CODE STM
 // Configure Tx buffer message 1
 TxHeader.Identifier = 0x1;
 TxHeader.IdType = FDCAN_STANDARD_ID;
 TxHeader.TxFrameType = FDCAN_DATA_FRAME;
 TxHeader.DataLength = FDCAN_DLC_BYTES_12;
 TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
 TxHeader.BitRateSwitch = FDCAN_BRS_ON;
 TxHeader.FDFormat = FDCAN_FD_CAN;
 TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
 TxHeader.MessageMarker = 0x0; // Ignore because FDCAN_NO_TX_EVENTS
 if(HAL_FDCAN_AddMessageToTxBuffer(&hfdcan1, &TxHeader, TxData_Node1_To_Node2, FDCAN_TX_BUFFER0) != HAL_OK)
 {
 	 Error_Handler();
 }
 
 // Configure Tx buffer message 2
	TxHeader2.Identifier = 0x10;
	TxHeader2.IdType = FDCAN_STANDARD_ID;
	TxHeader2.TxFrameType = FDCAN_DATA_FRAME;
	TxHeader2.DataLength = FDCAN_DLC_BYTES_12;
	TxHeader2.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
	TxHeader2.BitRateSwitch = FDCAN_BRS_ON;
	TxHeader2.FDFormat = FDCAN_FD_CAN;
	TxHeader2.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
	TxHeader2.MessageMarker = 0x0; // Ignore because FDCAN_NO_TX_EVENTS
	if(HAL_FDCAN_AddMessageToTxBuffer(&hfdcan1, &TxHeader2, TxData_Node1_To_Node22, FDCAN_TX_BUFFER1) != HAL_OK)
	{
	 Error_Handler();
	}

 //Configure standard ID reception filter to Rx buffer 0
 sFilterConfig.IdType = FDCAN_STANDARD_ID;
 sFilterConfig.FilterIndex = 0;
 #if 0
 sFilterConfig.FilterType = FDCAN_FILTER_DUAL; // Ignore because FDCAN_FILTER_TO_RXBUFFER
 #endif
 sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXBUFFER;
 sFilterConfig.FilterID1 = 0x700; // ID Node2
 #if 0
 sFilterConfig.FilterID2 = 0x0; // Ignore because FDCAN_FILTER_TO_RXBUFFER
 #endif
 sFilterConfig.RxBufferIndex = 0;

 if(HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
 {
 	 Error_Handler();
 }


 //Configure standard ID reception filter to Rx buffer 1
 sFilterConfig2.IdType = FDCAN_STANDARD_ID;
 sFilterConfig2.FilterIndex = 1;
 #if 0
 sFilterConfig2.FilterType = FDCAN_FILTER_DUAL; // Ignore because FDCAN_FILTER_TO_RXBUFFER
 #endif
 sFilterConfig2.FilterConfig = FDCAN_FILTER_TO_RXBUFFER;
 sFilterConfig2.FilterID1 = 0x2; // ID Node2
 #if 0
 sFilterConfig2.FilterID2 = 0x0; // Ignore because FDCAN_FILTER_TO_RXBUFFER
 #endif
 sFilterConfig2.RxBufferIndex = 1;

 if(HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig2) != HAL_OK)
 {
 	 Error_Handler();
 }


 // Start the FDCAN module
 if(HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
 {
 	 Error_Handler();
 }

 // Send Tx buffer message 1
 if(HAL_FDCAN_EnableTxBufferRequest(&hfdcan1, FDCAN_TX_BUFFER0) != HAL_OK)
 {
 	 Error_Handler();
 }

 // Send Tx buffer message 2
 if(HAL_FDCAN_EnableTxBufferRequest(&hfdcan1, FDCAN_TX_BUFFER1) != HAL_OK)
 {
 	 Error_Handler();
 }


 // Polling for transmission complete on buffer index 0
 while(HAL_FDCAN_IsTxBufferMessagePending(&hfdcan1, FDCAN_TX_BUFFER0) == 1);

 // Polling for reception complete on buffer index 0
 while(HAL_FDCAN_IsRxBufferMessageAvailable(&hfdcan1, FDCAN_RX_BUFFER0) == 0);

 // Polling for transmission complete on buffer index 1
 while(HAL_FDCAN_IsTxBufferMessagePending(&hfdcan1, FDCAN_TX_BUFFER1) == 1);

 // Polling for reception complete on buffer index 1
 while(HAL_FDCAN_IsRxBufferMessageAvailable(&hfdcan1, FDCAN_RX_BUFFER1) == 0);

 // Retrieve message from Rx buffer 0
 if(HAL_FDCAN_GetRxMessage(&hfdcan1, FDCAN_RX_BUFFER0, &RxHeader, RxData_From_Node2) != HAL_OK)
 {
 	 Error_Handler();
 }
 // Retrieve message from Rx buffer 1
	if(HAL_FDCAN_GetRxMessage(&hfdcan1, FDCAN_RX_BUFFER1, &RxHeader2, RxData_From_Node22) != HAL_OK)
	{
	Error_Handler();
	}
//FIN CODE STM

 /* USER CODE END 2 */

 

Model.cpp 

#include <fdcan.h>


extern FDCAN_RxHeaderTypeDef RxHeader;
extern FDCAN_TxHeaderTypeDef TxHeader;
extern uint8_t RxData_From_Node2[12];
extern uint8_t TxData_Node1_To_Node2[12];

extern FDCAN_RxHeaderTypeDef RxHeader2;
extern FDCAN_TxHeaderTypeDef TxHeader2;
extern uint8_t RxData_From_Node22[12];
extern uint8_t TxData_Node1_To_Node22[12];

 //ajout message au TXBuffer0
	 if(HAL_FDCAN_AddMessageToTxBuffer(&hfdcan1, &TxHeader, TxData_Node1_To_Node2, FDCAN_TX_BUFFER0) != HAL_OK)
	 {
		 //Error_Handler();
	 }
		// Send Tx buffer message 1
	 if(HAL_FDCAN_EnableTxBufferRequest(&hfdcan1, FDCAN_TX_BUFFER0) != HAL_OK)
	 {
		 //Error_Handler();
	 }
	 //ajout message au TXBuffer1
	 if(HAL_FDCAN_AddMessageToTxBuffer(&hfdcan1, &TxHeader2, TxData_Node1_To_Node22, FDCAN_TX_BUFFER1) != HAL_OK)
	 {
		 //Error_Handler();
	 }
		// Send Tx buffer message 2
	 if(HAL_FDCAN_EnableTxBufferRequest(&hfdcan1, FDCAN_TX_BUFFER1) != HAL_OK)
	 {
		 //Error_Handler();
	 }

	 // Retrieve message from Rx buffer 0
	 if(HAL_FDCAN_GetRxMessage(&hfdcan1, FDCAN_RX_BUFFER0, &RxHeader, RxData_From_Node2) != HAL_OK)
	 {
		 //Error_Handler();
	 }
	 // Retrieve message from Rx buffer 1
	 if(HAL_FDCAN_GetRxMessage(&hfdcan1, FDCAN_RX_BUFFER1, &RxHeader2, RxData_From_Node22) != HAL_OK)
	 {
		 //Error_Handler();
	 }