Skip to main content
Visitor II
Apr 9, 2025 2:20 PM UTC
Question

Failed to read ROM table via AP 3 - Failed to start GDB server

Dear community members,

I am using STM32CubeIDE to develop and debug the STM32H7 series dual-core microcontrollers, but I have encountered a stubborn problem and hope to get help and suggestions from the community.

### Problem description
I used the built-in example project GPIO for testing according to the application note AN5361(You can refer to the attached content).
I was able to successfully compile, burn and debug the program for the Cortex-M7 core, but when trying to debug the Cortex-M4 core, I always received the following error message:

```
Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
An error occurred while initializing the ST-Link device.

Reason: (255) Unknown reason. Please check the power supply and cable connected to the target machine.
```

More specifically, the debug console shows:

```
Failed to read ROM table via AP 3
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.
```

### Solutions I have tried

1. **Checked and configured option bytes**:

* Verified via STM32CubeProgrammer that BCM4 (CM4 boot option) is enabled

* NRST_STOP_D2 and NRST_STBY_D2 are also correctly enabled

* Boot address is also correctly configured (CM7: 0x08000000, CM4: 0x08100000)

2. **Debugger configuration**:

* CM7 configuration: Access port set to "0 - Cortex-M7", Reset behavior set to "Connect under reset"

* CM4 configuration: Access port set to "3 - Cortex-M4", Reset behavior set to "None"

Both configurations have "Enable shared ST-LINK" enabled
* CM4's port number is 3 higher than CM7 (CM7: 61234, CM4: 61237)
* ​​Download disabled in CM4's Startup tab (because CM7 is already responsible for downloading)
3. **Boot sequence** :
* Start a CM7 debug session and let it run
* Then try to start a CM4 debug session
* Make sure the CM7 code contains code to release the hardware semaphore to wake up the CM4
4. **Connection test** :
* Use STM32CubeProgrammer to successfully connect to the device and read memory
* ST-LINK firmware has been updated to the latest version
* Tried different USB cables and ports

### System information

* Development board model: [NUCLEO-H755ZI-Q]
* Chip: STM32H755
* STM32CubeIDE version: [1.18.0]
* ST-LINK version: [STLINK-V3 V3J16M7]
* Operating system: [Linux 22.04]

### Debug information

When CM7 debugging is successfully started, the program falls into a loop waiting for CM4 to start:
When executing GPIO_EXTI_CM7_Debug, the output information is:


STMicroelectronics ST-LINK GDB server. Version 7.10.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.

Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled

Info : default port : 7184
Info : Remote address: 127.0.0.1
Info : stlinkserver already running, exit
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------

 

Log output file: /tmp/STM32CubeProgrammer_q3TuDb.log
ST-Link Server is running on port : 7184
Info : default port : 7184
Info : Remote address: 127.0.0.1
Info : stlinkserver already running, exit
ST-LINK SN : 004400193433510A37363934
ST-LINK FW : V3J16M7
Board : NUCLEO-H755ZI-Q
Voltage : 3,29V
Info : default port : 7184
Info : Remote address: 127.0.0.1
Info : stlinkserver already running, exit
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
BL Version : 0x91

Opening and parsing file: ST-LINK_GDB_server_dxfKHW.srec


Memory Programming ...
File : ST-LINK_GDB_server_dxfKHW.srec
Size : 4.59 KB
Address : 0x08100000

 

Erasing memory corresponding to sector 0:
Erasing internal memory sector 8
Download in Progress:


File download complete
Time elapsed during download operation: 00:00:03.647

 

Verifying ...

 


Download verified successfully


Info : default port : 7184
Info : Remote address: 127.0.0.1
Info : stlinkserver already running, exit
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------

 

Log output file: /tmp/STM32CubeProgrammer_FY9gId.log
ST-Link Server is running on port : 7184
Info : default port : 7184
Info : Remote address: 127.0.0.1
Info : stlinkserver already running, exit
Info : default port : 7184
Info : Remote address: 127.0.0.1
Info : stlinkserver already running, exit
ST-LINK SN : 004400193433510A37363934
ST-LINK FW : V3J16M7
Board : NUCLEO-H755ZI-Q
Voltage : 3,29V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7/M4
BL Version : 0x91

Opening and parsing file: ST-LINK_GDB_server_4APDtX.srec


Memory Programming ...
File : ST-LINK_GDB_server_4APDtX.srec
Size : 8.66 KB
Address : 0x08000000

 

Erasing memory corresponding to sector 0:
Erasing internal memory sector 0
Download in Progress:


File download complete
Time elapsed during download operation: 00:00:03.837

 

Verifying ...

 


Download verified successfully


Info : default port : 7184
Info : Remote address: 127.0.0.1
Info : stlinkserver already running, exit

 

When executing GPIO_EXTI_CM4_Debug, the output information is as follows:

STMicroelectronics ST-LINK GDB server. Version 7.10.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.

Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61240
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled

Info : default port : 7184
Info : Remote address: 127.0.0.1
Info : stlinkserver already running, exit
Failed to read ROM table via AP 3

Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.


My questions

1. Why can't I access CM4 through AP 3 even though the BCM4 option is enabled?

2. Are there any other configurations or settings that may affect dual-core debugging?

3. Are there any specific debugging commands or methods to get more detailed error information?

4. Is this issue related to a specific STM32H7 model or development board?

If any additional information is needed, please feel free to contact me!
Any help or suggestions are greatly appreciated!

This topic has been closed for replies.

1 reply

ST Technical Moderator
Apr 25, 2025 8:47 AM UTC

Hello @hang 

Could you please check this thread? It seems like the same issue you are facing.

BR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.