Skip to main content
Associate II
November 21, 2023
Question

Failed to get the debug messages output (ST-LINK attached UART) of STM32H750B-DK

  • November 21, 2023
  • 3 replies
  • 1489 views

I use STM32H750B-DK board. It has UART3 connected to the ST-LINK USB.

I tried
uint8_t Test[] = "Hello World !!!\r\n";
HAL_UART_Transmit(&huart3,Test,sizeof(Test),10);
printf("Hello World 1 !!!\r\n");

HAL_UART_Transmit output has passed to the terminal.
printf doesn't print anything.
syscalls.c defines 
extern int __io_putchar(int ch) __attribute__((weak));
The implementation is hidden and it definitely doesn't deal with the UART3.

The actual function used in the printf implementation is:

__attribute__((weak)) int _write(int file, char *ptr, int len)
{
 (void)file;
 int DataIdx;


// UART3_TX((uint8_t *)ptr, len, 1000);

 for (DataIdx = 0; DataIdx < len; DataIdx++)
 {
 __io_putchar(*ptr++);
 }

 return len;
}


I redefined the weak _write() in the main.c

int _write(int file, char *data, int len)
{
 if ((file != STDOUT_FILENO) && (file != STDERR_FILENO))
 {
 errno = EBADF;
 return -1;
 }

 // arbitrary timeout 1000
 HAL_StatusTypeDef status =
 HAL_UART_Transmit(&huart3, (uint8_t*)data, len, 1000);

 // return # of bytes written - as best we can tell
 return (status == HAL_OK ? len : 0);
}


Surprise!!!
Breakpoint in main.c defined _write() has not hit. The weak _write() of syscalls.c continues working.

I tried a dirty solution.
Defined in the main.c following function:
HAL_StatusTypeDef UART3_TX(uint8_t *data, uint16_t len, uint32_t Timeout)
{
     return HAL_UART_Transmit(&huart3, data, len, Timeout);
}
I tried to call the function In the syscalls's version of the _write. The linker doesn't see UART3_TX().

What is going on? How can I make my debug output working?
Why it became unexpectedly complicated?

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    November 21, 2023

    The linker is pretty methodical, you're going to need to look at what it is being fed as input, and what the .MAP describes in the resultant output.

    Kind of suggests that syscalls.c isn't being pulled in.

    use strlen() not sizeof() for strings, with trailing NULs

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    tarbalAuthor
    Associate II
    November 21, 2023

    Thank you.
    This response doesn't help me getting printf working.

    tarbalAuthor
    Associate II
    November 21, 2023

    I found the mistake. The  _write() in the main.c does redefine _write() in the syscalls and the printf works. No help is required anymore.