Skip to main content
Visitor II
Dec 2, 2024 3:56 AM UTC
Question

Failed to execute MI command: load /[user/]/[Project]/STM32CubeIDE/Appli/Debug/Template_XIP_Appli.elf

Using STM32H7S78-DK board with a STM32CubeIDE project that utilizes an external memory loader, which is included in the project structure. when running debug I am getting a failure with the following console output: 

 

 

Error in final launch sequence:

Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Appli/Debug/Template_XIP_Appli.elf 

Error message from debugger back end:
Load failed ,Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Boot/Debug/Template_XIP_Boot.elf 

Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Appli/Debug/Template_XIP_Appli.elf 

Error message from debugger back end:
Load failed ,Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Boot/Debug/Template_XIP_Boot.elf 

Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Appli/Debug/Template_XIP_Appli.elf 

Error message from debugger back end:
Load failed
Load failed
Failed to execute MI command:
load /[User]/[Project]/STM32CubeIDE/Boot/Debug/Template_XIP_Boot.elf 

Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation

 

 

 Similar forum posts have recommended actions such as running the project with BOOT0 set, clearing out the flash memory with cubeprogrammer, and running the reset behavior as None. None of these have been successful or changed the error message. Console output is below, asking for any help or recommendation on how to resolve this error? Running STMCubeIDE on ubunutu LTS 20.04 

 

 

STMicroelectronics ST-LINK GDB server. Version 7.8.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.

Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 InitWhile : Enabled

Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.17.0 
 -------------------------------------------------------------------

Warning: The external loader file does not exist:
Template_XIP_ExtMemLoader.stldr
Encountered Error when opening /opt/st/stm32cubeide_1.16.0/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_2.1.400.202404281720/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Shutting down...
Exit.

 

 



This topic has been closed for replies.

1 reply

MM..1
Super User
Dec 7, 2024 8:31 AM UTC

Start with complete simple project only for internal flash. In your log is reported missed file for load external flash on DK. Optimal is close IDE and all, and open only Programmer GUI. First step is upgrade onboard STLINK. After this try connect and read MCU.