Skip to main content
Leopold N.
Associate II
September 7, 2022
Question

Failed to execute MI command: -data-disassemble -s 484 -e 760 -- 3 Error message from debugger back end: Cannot access memory at address 0x10000

This Error shows up on various Places in the Memory. I can access the Memory through the Memory Browser, but unfortunately there is no Disassembly Interpretation like in the Disassembly Window. This Errors occurs mainly on SRAM Memory, not in Flash. And it really slows down the Code Execution while Debugging, because it tries to fetch the Data the whole Time and blocks the Debugging itself.

Would be nice if there is a Fix for this.0693W00000Suj1xQAB.png

This topic has been closed for replies.