Skip to main content
Visitor II
July 15, 2024
Solved

Ethernet Based Application in H755ZI-Q board using LwIP -TCP communication particularly for RMII support

  • July 15, 2024
  • 1 reply
  • 1337 views

Hello community! We are trying to develop an application based on Ethernet using  LwIP stack in STM32H755ZI-Q nucleo board which supports only RMII mode of configuration. We need a communication to be based on TCP protocol. For this we need some solutions for how to enable the required modules and functions in generated files and please suggest us the example files to transmit and receive the data via ethernet from board to board, board to PC or Board to PLC (Especially the functions and how to configure and pass the function parameters with data). 

    This topic has been closed for replies.

    1 reply

    STeaBest answer
    ST Employee
    July 22, 2024
    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.