Error while flashing GPIO_EXTI program on STM32F746ZG board
- 1 reply
- 1397 views
Not able to flash GPIO_EXTI program on STM32F746ZG board using CubeIDE tool
Source code : https://github.com/STMicroelectronics/STM32CubeF7/tree/master/Projects/STM32F746ZG-Nucleo/Examples/GPIO/GPIO_EXTI
Environment : Ubuntu 18.04.4 LTS
Cube IDE : STM32CubeIDE Version: 1.3.1 Build: 6291_20200406_0752 (UTC)
CubeMX : STM32CubeMX - STM32 Device Configuration Tool Version: 5.6.1-RC1 Build: 20200405-2303 (UTC)
ST Link Version : V2J36M26
Log Status :
/home/default/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Projects/STM32F746ZG-Nucleo/Examples/GPIO/GPIO_EXTI/SW4STM32/STM32746ZG_Nucleo/Debug/st-link_gdbserver_log.txt
[0.000] initConfigParams(): Configuration flags start
[0.000] initConfigParams(): external-init false
[0.000] initConfigParams(): pend-halt-timeout (null)
[0.000] initConfigParams(): halt false
[0.000] initConfigParams(): config-file ""
[0.000] initConfigParams(): persistent false
[0.000] initConfigParams(): +log-file "/home/default/STM32Cube/Repository/STM32Cube_FW_F7_V1.16.0/Projects/STM32F746ZG-Nucleo/Examples/GPIO/GPIO_EXTI/SW4STM32/STM32746ZG_Nucleo/Debug/st-link_gdbserver_log.txt"
[0.000] initConfigParams(): +log-level 31
[0.000] initConfigParams(): +port-number 61234
[0.000] initConfigParams(): +verbose true
[0.000] initConfigParams(): refresh-delay 15
[0.000] initConfigParams(): +verify true
[0.000] initConfigParams(): +swd true
[0.000] initConfigParams(): swo-port 61234
[0.000] initConfigParams(): cpu-clock 8000000
[0.000] initConfigParams(): swo-clock-div 128
[0.000] initConfigParams(): initialize-reset false
[0.000] initConfigParams(): debuggers false
[0.000] initConfigParams(): serial-number ""
[0.000] initConfigParams(): +apid 0
[0.000] initConfigParams(): +attach true
[0.000] initConfigParams(): shared false
[0.000] initConfigParams(): erase-all false
[0.000] initConfigParams(): memory-map ""
[0.000] initConfigParams(): ext-memory-loaders false
[0.000] initConfigParams(): extload ""
[0.000] initConfigParams(): +stm32cubeprogrammer-path "/opt/st/stm32cubeide_1.3.0/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_1.3.0.202002181050/tools/bin"
[0.000] initConfigParams(): temp-path ""
[0.000] initConfigParams(): preserve-temps false
[0.000] initConfigParams(): frequency -1
[0.000] initConfigParams(): licenses false
[0.000] initConfigParams(): ignore-rest false
[0.000] initConfigParams(): version false
[0.000] initConfigParams(): help false
[0.000] initConfigParams(): Configuration flags end
[0.000] init(): STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
[0.003] Device_Initialise(): Target connection mode: Attach
[0.007] reset_hw_wtchpt_module(): Hardware watchpoint supported by the target
[0.010] Device_Initialise(): COM frequency = 4000 kHz
[0.010] Device_Initialise(): ST-LINK Firmware version : V2J36M26
[0.010] Device_Initialise(): Device ID: 0x449
[0.010] Device_Initialise(): PC: 0x0
[0.010] Device_GetStatus(): ST-LINK device status: RUN_MODE
[0.011] Device_Initialise(): ST-LINK detects target voltage = 3.25 V
[0.011] Device_Initialise(): ST-LINK device status: RUN_MODE
[0.011] initServerContext(): ST-LINK device initialization OK
[0.011] WaitConnection(): Waiting for connection on port 61234...
[2.028] WaitConnection(): Accepted connection on port 61234...
[2.029] haltOnConnect(): Try halt...
[11.718] haltOnConnect(): Halt timeout (0s) exceeded.
Exception Details : Error in final launch sequence:
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
Remote communication error. Target disconnected.: Connection reset by peer.
Failed to execute MI command:
target remote localhost:61234
Error message from debugger back end:
Remote communication error. Target disconnected.: Connection reset by peer.
Remote communication error. Target disconnected.: Connection reset by peer.