Skip to main content
Associate II
Apr 14, 2026 2:50 PM UTC
Question

error updating STM32CubeIDE 2.1.1

error updating STM32CubeIDE 2.1.1 see attachment.

6 replies

Andrew Neil
Super User
Apr 14, 2026 3:06 PM UTC

Rather than update, have you tried just doing a from-scratch install of the new version?

It is fine to have multiple versions installed at the same time, provided that you:

  1. Install each into a separate folder;
  2. Use a separate workspace (or workspaces) for each

 

PS:

It also has the advantage that, if you encounter some problem/incompatibility with the new version, you still have the old version where you can continue working ...

This is why I never upgrade - always install the new one from scratch.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ST Technical Moderator
Apr 14, 2026 3:09 PM UTC

Hello @@BrucePB 

Let me thank for posting.

For more investigation, could you provide please which STM32CubeIDE version you are using.

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
BrucePBAuthor
Associate II
Apr 16, 2026 11:42 PM UTC

Hi Mahmoud,

I thought  I replier but I do not see it in the thread.

The About says I am using Version: 2.0.0

The update is trying to go to  2.1.1

PS - I am using Windows 10.

ST Technical Moderator
Apr 20, 2026 10:07 AM UTC

Hello @BrucePB 

I reproduced the test and the STM32CubeIDE update was successful.

I recommend that you delete the cache folders [.stm32cubeide, .stm32cubemx, .stm32cubefinder] under this path:

C:\Users\, set the network connection and relaunch the update process.

Thanks.

Mahmoud

 

 

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.