Skip to main content
RBamf.1
Associate III
Mar 19, 2023 4:47 PM UTC
Question

Error trying to launch STM32CubeIDE on linux!

I have installed the STM32CubeIDE 1.12.0 from the STM32 official website onto my Arch Linux laptop but when i try to launch it, it closes and reports an error after the splash screen.

I have searched on pacman (the arch package manager) for stm32cubeide too, but they are having the same error too. See the comments section on https://aur.archlinux.org/packages/stm32cubeide

Here is the error:

[ri@r Desktop]$ /opt/st/stm32cubeide_1.12.0/stm32cubeide_wayland
SWT WebKitGDBus: error creating DBus server Error binding to address (GUnixSocketAddress): No such file or directory
SWT WebKit: error initializing DBus server, dBusServer == 0
 
(STM32CubeIDE:9473): GLib-GIO-CRITICAL **: 16:40:15.499: g_dbus_server_get_client_address: assertion 'G_IS_DBUS_SERVER (server)' failed
#
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0x00007fd88683ed16, pid=9473, tid=9474
#
# JRE version: OpenJDK Runtime Environment Temurin-11.0.17+8 (11.0.17+8) (build 11.0.17+8)
# Java VM: OpenJDK 64-Bit Server VM Temurin-11.0.17+8 (11.0.17+8, mixed mode, tiered, compressed oops, g1 gc, linux-amd64)
# Problematic frame:
# C [libswt-gtk-4950r5.so+0x3ed16] Java_org_eclipse_swt_internal_C_strlen+0xf
#
# Core dump will be written. Default location: Core dumps may be processed with "/usr/lib/systemd/systemd-coredump %P %u %g %s %t %c %h" (or dumping to /home/richard/Desktop/core.9473)
#
# An error report file with more information is saved as:
# /home/r/Desktop/hs_err_pid9473.log
Compiled method (nm) 9481 5616 n 0 org.eclipse.swt.internal.C::strlen (native)
 total in heap [0x00007fd917d3c190,0x00007fd917d3c530] = 928
 relocation [0x00007fd917d3c308,0x00007fd917d3c338] = 48
 main code [0x00007fd917d3c340,0x00007fd917d3c528] = 488
 oops [0x00007fd917d3c528,0x00007fd917d3c530] = 8
Compiled method (nm) 9486 5616 n 0 org.eclipse.swt.internal.C::strlen (native)
 total in heap [0x00007fd917d3c190,0x00007fd917d3c530] = 928
 relocation [0x00007fd917d3c308,0x00007fd917d3c338] = 48
 main code [0x00007fd917d3c340,0x00007fd917d3c528] = 488
 oops [0x00007fd917d3c528,0x00007fd917d3c530] = 8
#
# If you would like to submit a bug report, please visit:
# https://github.com/adoptium/adoptium-support/issues
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#

And the error report file is attached below.

This topic has been closed for replies.

40 replies

Janek1
Associate II
Apr 11, 2023 2:44 PM UTC

Installing the webkitgtk-6.0 package solved this issue for me on Arch.

JHenz.1
Visitor II
May 1, 2023 4:32 PM UTC

Having the identical error on Fedora 38 using both the generic install and the RPM. I have  webkit2gtk4.1 installed and get the same dump

Janek1
Associate II
May 4, 2023 2:29 PM UTC

Update on this (with some solutions i found in the AUR comments / forum):

The issue is indeed in an incompatibility in webkit2gtk and eclipse. In an earlier post i said that installing webkitgtk-6.0 solved the issue, seems like it didn't.

But i have found a new solution which is removing webkit2gtk from your system (has to be done with pacman -Rdd otherwise cubeide will be removed as well). This breaks browser functionality in eclipse (which i don't really know what its supposed to be and have probably never used, so yea i'm fine with that). Someone else mentioned swapping webkit2gtk for chromium, which i guess could work, but i didn't bother trying. If you're interested in this you can probably find the comment (which also contained a link) in the comments of the AUR package.

PGump.1
Senior II
May 9, 2023 1:57 AM UTC

Hello,

I want to start working with STM32WB55 micros.

Some time ago, with much trial-and-error, I installed STM32CubeIDE V1.8.0 on to my Suse-tumbleweed computer. It mostly works well (ask me for details if you want to know more). This installation type DOES NOT allow updates.

I downloaded STMCubeIDE V1.12.1 (generic linux), and installed it the same manner as above. It installs without complaining. But it does NOT run - it seems to start okay, prompts me for the "workspace", but shortly after java dies...

My java version is:-

openjdk 17.0.7 2023-04-18

OpenJDK Runtime Environment (build 17.0.7+0-suse-1.1-x8664)

OpenJDK 64-Bit Server VM (build 17.0.7+0-suse-1.1-x8664, mixed mode, sharing)

My STM32CubeIDE V1.8.0 still works as it did.

Can anyone help me?

Thanking you

Pedro

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.
squiggle
Graduate II
May 9, 2023 3:35 AM UTC

I can help. And I say this in the most serious, sincere, and non-sarcastic way possible.

Get rid of STM32CubeIDE and any other Eclipse-based IDE. Install VSCode or Geany or literally any other IDE besides Eclipse. Then install and use STM32CubeMX to generate your code to load into the better IDE.

PGump.1
Senior II
May 9, 2023 6:08 AM UTC

Thanks for your comments @squiggle. It may come to that...

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.
AKoch.6
Visitor II
May 11, 2023 9:12 AM UTC

Seems to be same issue:

community.st.com/s/question/0D53W00002FDNNJSA5/can-no-longer-create-a-new-workspace-stm32cubeide-1121

AKoch.6
Visitor II
May 11, 2023 9:58 AM UTC

Marcelo Jimenez Shellscript (fix_stm32cubeide) worked for me

PGump.1
Senior II
May 12, 2023 1:41 AM UTC

Thanks @AKoch.6, "fix_stm32cubeide" fixed it for me too. :grinning_face:

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.
Jun 10, 2023 5:23 PM UTC

I had the same issue and this line of the error message caught my eye:

SWT WebKitGDBus: error creating DBus server Error binding to address (GUnixSocketAddress): No such file or directory

I looked into the source code of SWT to find out where this error happens. I saw it wants to open a directory named 

/tmp/SWT-GDBusServer

 and throws the error if it doesn't exist. so I manually created this directory and to my surprise it fixed the issue.

mkdir '/tmp/SWT-GDBusServer'

Explorer
Jun 16, 2023 10:21 PM UTC

thank you so much, creating the missing folder

fixed the problem i can now succesfully launch the last version !

the fix was surprisingly really easy