Skip to main content
DCorn
Associate II
June 21, 2019
Question

Error programming STM32H743 Nucleo board with STM32CubeIDE

Hi,

I get an error when trying to program nucleo board with the STM32H743 and STMCubeIDE with any of the example projects. They compile OK but I get an error while programming the board.

It works with IAR, 

the error message is

STMicroelectronics ST-LINK GDB server. Version 5.2.3

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

Waiting for debugger connection...

Debugger connected

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.1.0          

   -------------------------------------------------------------------

Log output file:  C:\Users\smith\AppData\Local\Temp\STM32CubeProgrammer_a01452.log

ST-LINK SN : 0672FF383930434B43184445

ST-LINK FW : V2J31M21

Voltage   : 3.24V

SWD freq  : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x450

Device name : STM32H7xx

Flash size : 2 MBytes

Device type : MCU

Device CPU : Cortex-M7

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a01452.srec

 File     : ST-LINK_GDB_server_a01452.srec

 Size     : 136080 Bytes

 Address    : 0x08000000 

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 1]

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:03.253

Verifying ...

Download verified successfully 

Target unknown error 19

Error in initializing ST-LINK device.

Reason: Unknown. Please check power and cabling to target.

Failed to restart ST-LINK connection

Error in STM32CubeProgrammer

Target is not responding, retrying...

This topic has been closed for replies.

4 replies

Markus GIRDLAND
ST Employee
June 25, 2019

Could you enable to gdbserver log and paste it? It's located in the Debugger tab of the debug configuration, a box at "Log to file:".

DCorn
DCornAuthor
Associate II
June 26, 2019

please find attached log below

Markus GIRDLAND
ST Employee
June 26, 2019

This looks a bit strange. The error seems to get generated as soon as CubeProgrammers flash has been completed.

If you first start a debug session as usual (or try to) and then after the first time where it supposedly flashed OK you go into your debug configuration and then into your "Startup" tab and uncheck the "Load image" box and hit "Debug". Can you start a debug session then?

Also, what happens if you choose OpenOCD as the debug probe? (In the Debugger tab)

DCorn
DCornAuthor
Associate II
June 27, 2019

OpenOCD did not work

Unchecking "Load Image" it starts a debug session OK.