Skip to main content
Associate II
September 16, 2024
Question

Error no such file or directory during validation on target with stm cube AI

Hello,

I'm trying to validate on target a CNN neural network in stm cube IDE (the target is the board STEVAL-STWINKT1B) but I alwais find an error:

C:/ST/STM32CubeIDE_1.16.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: cannot find -l:NetworkRuntime900_CM4_GCC.a: No such file or directory 
collect2.exe: error: ld returned 1 exit status 
make: *** [Makefile:85: Debug/mxAI1769727189411900.elf] Error 1 
Automatic build and run failed

The validation on desktop run well but the validation on target return this error both with random data in input and with data entered manually.

I'm working with this network:

https://drive.google.com/file/d/1FizAT25KlB1PKellG3EwzSmL5bcMf7Kx/view?usp=sharing

    This topic has been closed for replies.

    1 reply

    Luca4Author
    Associate II
    September 16, 2024

    P.S.

    in the initial network configuration I inserted low compression so as not to exceed the available flash.