Skip to main content
m4l490n
Associate III
Jun 12, 2024 5:35 AM UTC
Question

Error installing SMT32CubeIDE 1.15.1 in Ubuntu 22.04

I'm getting the following error when trying to install STM32CubeIDE in Ubuntu 22.04:

dpkg: error processing archive /home/m4l490n/Downloads/makeself_dir_Dg5j3M/segger-jlink-udev-rules-7.94h-linux-all.deb (--unpack):
trying to overwrite '/etc/udev/rules.d/99-jlink.rules', which is also in package jlink 7.9611
Errors were encountered while processing:
/home/m4l490n/Downloads/makeself_dir_Dg5j3M/segger-jlink-udev-rules-7.94h-linux-all.deb
N: Download is performed unsandboxed as root as file '/home/m4l490n/Downloads/makeself_dir_Dg5j3M/segger-jlink-udev-rules-7.94h-linux-all.deb' couldn't be accessed by user '_apt'. - pkgAcquire::Run (13: Permission denied)
E: Sub-process /usr/bin/dpkg returned an error code (1)

Does anyone have an idea of what's going on?

2 replies

Visitor II
Jan 17, 2026 2:06 PM UTC

I have the same problem with stm32ide 1.19 and ubuntu 22.04.

Even if deleting the /etc/udev/rules.d/99-jlink file the error stays the same

Visitor II
Jan 17, 2026 2:42 PM UTC

For me the solution was to remove a former jlink package with

sudo dpkg -r --force-depends jlink

then the installation ran without problems