Skip to main content
Senior
Feb 5, 2025 11:43 AM UTC
Solved

Error in final launch sequence - No device on target

I have a NUCLEO-G491RE board connected to a PC running STM32CubeIDE v1.17.0. On first connection I was prompted to update the firmware on the board, which I did. On successful completion of the update I disconnected and reconnected the board, but the download failed with the attached message. 

I have tried several USB cables and also with and without an intermediate USB hub to eliminate these possibilities.

What is the solution please?

This topic has been closed for replies.
alwBest answer
Senior
Feb 8, 2025 2:12 AM UTC

Problem solved, it was just jumper link settings.

JP5 (5V_SEL): 5V_STLK

JP6 (IDD):        On

JP7 (BOOT0):  Off

Suggestion, rather than the error messages that are provided, have ones that advise users to check thatthese links are correctly fitted.

11 replies

ST Technical Moderator
Feb 6, 2025 8:08 AM UTC

Hello @alw ,

First let me thank you for posting.

For more investigation, I suggest please that you provide your STM32CubeIDE Project.

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
alwAuthor
Senior
Feb 6, 2025 8:50 AM UTC

Hi Mahmoud,

Please see attached, a simple enough program that builds ok, just can't run it on the target NUCLEO-G491RE board after updating the firmware on it. Is there a way of manually reflashing the STLink firmware to the NUCLEO board please?

Kind regards,

Al

alwAuthor
Senior
Feb 6, 2025 2:45 PM UTC

Hi Mahmoud,

I hit the limit on private messages.  

The only issue I have is that I can't run the application without launching debug, even with selecting Run As STM32C/C++ Application. How do I run without activating debug please?

 

STMicroelectronics ST-LINK GDB server. Version 7.9.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

-------------------------------------------------------------------

STM32CubeProgrammer v2.18.0

-------------------------------------------------------------------

 

 

 

Log output file: C:\Users\al_wa\AppData\Local\Temp\STM32CubeProgrammer_a02844.log

ST-LINK SN : 0039003C3133511237363734

ST-LINK FW : V3J15M7

Board : NUCLEO-G474RE

Voltage : 3.28V

SWD freq : 24000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x469

Revision ID : Rev X

Device name : STM32G47x/G48x/G414

Flash size : 512 KBytes

Device type : MCU

Device CPU : Cortex-M4

BL Version : 0xD5

Debug in Low Power mode enabled

 

Opening and parsing file: ST-LINK_GDB_server_a02844.srec

 

 

Memory Programming ...

File : ST-LINK_GDB_server_a02844.srec

Size : 11.86 KB

Address : 0x08000000

 

 

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 5]

Download in Progress:

 

 

File download complete

Time elapsed during download operation: 00:00:00.326

 

 

 

Verifying ...

 

 

 

 

Download verified successfully

 

 

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Shutting down...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

 

 

alwAuthor
Senior
Feb 7, 2025 10:04 AM UTC

Hi Mahmoud,

I just got the same message about hitting the limit again on private messages

Following one of the other posts I deleted the existing .metadata folder in the workspace so that a new one would be created on launching STM32CubeIDE. I build a simple application based on my Nucleo board (just changing LPUART1 baud rate) and again try to Run As STM32 C/C++ Application. All I want to do download and run the application to the target hardware without invoking the debugger, I never had these problems with previous versions of STM32CubeIDE.

 

STMicroelectronics ST-LINK GDB server. Version 7.9.0

Copyright (c) 2024, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

 

ST-LINK Failed to get target status

 

Error in initializing ST-LINK device.

Reason: Unknown. Please check power and cabling to target.

alwAuthor
Senior
Feb 7, 2025 10:05 AM UTC

..

alwAuthor
Senior
Feb 7, 2025 10:06 AM UTC

Jumper link is on 5V_STLK

alwAuthor
Senior
Feb 7, 2025 10:08 AM UTC

And despite the error message I can upgrade the ST-Link as before, so the cable etc. is ok.

ST Technical Moderator
Feb 7, 2025 1:12 PM UTC

Hello @alw ,

Further to your comment, I was able to launch the debug session using the STM32CubeIDE Project that you have attached.

MahmoudBenRomdhane_0-1738933850301.png

I suggest please that you provide the debug configuration.

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
alwAuthor
Senior
Feb 7, 2025 1:46 PM UTC

Hi Mahmoud,

I've attached a screen capture of the debug configuration and also having cleared out my workspace, a zip file of that containing the one project, as deleting the previous .metadata folder changed the run sequence such that the GDB server doesn't start.

250207_Debug_Configuration.png

ST Technical Moderator
Feb 7, 2025 3:47 PM UTC

Hello @alw ,

Further to the picture provided on message. I recommend that you change the jumper on CN11 to JP6.

IMG_2178.jpeg

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
alwAuthorBest answer
Senior
Feb 8, 2025 2:12 AM UTC

Problem solved, it was just jumper link settings.

JP5 (5V_SEL): 5V_STLK

JP6 (IDD):        On

JP7 (BOOT0):  Off

Suggestion, rather than the error messages that are provided, have ones that advise users to check thatthese links are correctly fitted.