Skip to main content
MPast.1
Senior
July 27, 2021
Question

ERROR: Couldn't parse external memory loader

Hi everyones,

I have a little (but big) problem with customized external loader.

The compiler report this error: " ERROR: Couldn't parse external memory loader"

0693W00000D0o2sQAB.jpgStm32 Cubeprogrammer instead, tell me everything is OK.

I tried to download a simple file inside my QSPI external memory and it works correctly.

0693W00000D0o37QAB.jpgI don't what's the problem in stm32 IDE.

Does someone has some hints or idea?

Second question:

Why I see only one custom loader on IDE instead of two, like on windows folder?

0693W00000D0o3lQAB.jpg 

0693W00000D0o3gQAB.jpgThe result not change also after a reboot of the IDE?

I'm using the latest IDE version:

0693W00000D0o4KQAR.jpg 

Thanks in advance

Best regards.

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
July 27, 2021

>>Stm32 Cubeprogrammer instead, tell me everything is OK.

Seems to be operating on Internal Memory

>>ERROR: Couldn't parse external memory loader

Seems to be a complaint about the form/structure of the ELF file, and the StorageInfo within.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Emilmart
Associate III
August 3, 2021

Hi I have the same problem since updating to STM32Cube IDE 1.7.0. My external loader worked perfectly on 1.6.0. Any idea ??

If I downgrade back to 1.6.0 it works again.

Also, after installing STM32Cube IDE 1.7.0, there is no folder "STM32CubeIDE_1.7.0" in C:\ST.

My .stdlr files are still in C:\ST\STM32CubeIDE_1.6.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.6.0.202101291314\tools\bin\ExternalLoader but it seems that STM32Cube IDE 1.7.0 use the .stldr in that exact same folder

Markus GIRDLAND
ST Employee
August 6, 2021

Hello!

Could you activate the gdb server log in your debug configuration, try to launch and then send the log to me?

SPerv.1
Associate
February 9, 2022

I have the same problem I upgraded from version 1.5 to 1.8. I have the same problem I upgraded from version 1.5 to 1.8. How can I fix it?

Here is the log:

[0.000] initConfigParams(): Configuration flags start

[0.000] initConfigParams():  external-init         false

[0.000] initConfigParams():  pend-halt-timeout       (null)

[0.000] initConfigParams():  halt              false

[0.000] initConfigParams():  config-file          ""

[0.000] initConfigParams():  persistent           false

[0.000] initConfigParams(): +log-file            "G:\projects\Tablet\src\Tablet_cerberus\Debug\st-link_gdbserver_log.txt"

[0.000] initConfigParams(): +log-level           31

[0.001] initConfigParams(): +port-number          61234

[0.002] initConfigParams(): +verbose            true

[0.002] initConfigParams():  refresh-delay         15

[0.003] initConfigParams(): +verify             true

[0.003] initConfigParams(): +swd              true

[0.004] initConfigParams(): +swo-port            61235

[0.004] initConfigParams():  cpu-clock           8000000

[0.005] initConfigParams():  swo-clock-div         128

[0.005] initConfigParams(): +initialize-reset        true

[0.005] initConfigParams():  debuggers           false

[0.006] initConfigParams(): +serial-number         "53FF6D065078485744440487"

[0.006] initConfigParams(): +apid              0

[0.007] initConfigParams():  attach             false

[0.007] initConfigParams():  shared             false

[0.008] initConfigParams():  erase-all           false

[0.008] initConfigParams():  memory-map           ""

[0.009] initConfigParams():  ext-memory-loaders       false

[0.009] initConfigParams(): +extload            "QSPI_flashloader_CSP.stldr"

[0.010] initConfigParams(): +stm32cubeprogrammer-path    "C:\ST\STM32CubeIDE_1.5.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.100.202110141430\tools\bin"

[0.011] initConfigParams():  temp-path           ""

[0.011] initConfigParams():  preserve-temps         false

[0.012] initConfigParams():  frequency           -1

[0.012] initConfigParams():  licenses            false

[0.013] initConfigParams():  ignore-rest          false

[0.013] initConfigParams():  version            false

[0.014] initConfigParams():  help              false

[0.014] initConfigParams(): Configuration flags end