Skip to main content
Associate III
May 30, 2025
Solved

Enabling printf on NUCLEO-N657 in STM32CubeIDE

I have enabled Serial Wire Viewer (SWV) in my m55 application as I have done with my m4 and m33 projects, but the printf is not appearing in the SWV view.

Are there additional setup required on the NUCLEO-N657 board such as jumper settings or additional software setup?

Thank you.

This topic has been closed for replies.
kag_embeddedBest answer
Associate III
May 30, 2025

@KDJEM.1 Thank you. Dividing the CPU clock by 8 resolved my issue.

2 replies

KDJEM.1
ST Technical Moderator
May 30, 2025

Hello @kag_embedded;

Could you please make sure that you:

- Enable TRACE CLOCK AND DEBUG CLOCK in DBGMCU register

- The SWV core clock in STM32CUBEIDE should always be CPU clock/8

- Configure the SWV ITM Data console

KDJEM1_0-1748614081081.png

KDJEM1_1-1748614093012.png

KDJEM1_2-1748614117827.png

Below an code example of printf:

################CODE BEGIN####################

int __io_putchar(int ch)
 {
 ITM_SendChar(ch);
 return(ch);
 }


int main(void)
{
 GPIO_InitTypeDef gpio_init;

DBGMCU->CR |=0x00300000;
 ITM->TER |= 0x1;
 ITM->TCR |= 0x00001;

 //SWO is Ball U12 or PB5 label on N6
 __HAL_RCC_GPIOB_CLK_ENABLE();
 gpio_init.Mode = GPIO_MODE_AF_PP;
 gpio_init.Pull = GPIO_PULLUP;
 gpio_init.Speed = GPIO_SPEED_FREQ_HIGH;
 gpio_init.Pin = GPIO_PIN_5;
 gpio_init.Alternate = GPIO_AF0_TRACE;
 HAL_GPIO_Init(GPIOB, &gpio_init);


 HAL_Init();

 /* Initialize LED1 */
 BSP_LED_Init(LED_GREEN);

 while (1)
 {
 /* Toggle LED1 every 500ms */
 BSP_LED_Toggle(LED_GREEN);
 HAL_Delay(500);
 printf("Hello world\n");
 }
}

################CODE END####################

 

For more information about  Serial Wire Viewer I recommend you to look at AN4948 precisely section "7.3 Printf via SWO/SWV"

If you want also to see the UART output message on the HyperTerminal, I recommend you to look at UART_Printf example. 

I hope this help you.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
kag_embeddedAuthorBest answer
Associate III
May 30, 2025

@KDJEM.1 Thank you. Dividing the CPU clock by 8 resolved my issue.