Question
EEPROM emulation in STM32F40x/STM32F41x microcontrollers (AN3969) - Needs to be updated!
Software obtained at this address, cannot be used directly with the STM32CubeIDE.
Strangely, current functions no longer have error control.
For example (Code available in the year: 2012:(
FLASH_Status FLASH_EraseSector(uint32_t FLASH_Sector, uint8_t VoltageRange)- Note: FLASH Status
Code available in the year: 2017 (From STM32CubeIDE, file: stm32f4xx_hal_flash_ex.c):
void FLASH_Erase_Sector(uint32_t Sector, uint8_t VoltageRange)When trying to adapt the code, I realized that there was a very significant reduction in the code, is this really necessary? Is it currently necessary to disregard the error tracking code that already existed?