Skip to main content
CTapp.1
Senior III
Apr 22, 2025 2:50 PM UTC
Solved

Duplicate system_stm32g0xx.c file after regenerating

I've got a project that has the following files in the tree view:

CTapp1_1-1745333196183.png

All is well if I clean and build, but if I open the .ioc and "Generate Code", the tree changes to:

CTapp1_2-1745333269644.png

and the project then fails to build due to a duplicate system_stm32g0xx.c file.

Why is this getting added and how do I stop it?

I am using STM32CubeIDE V1.18.1.

This topic has been closed for replies.
CTapp.1
CTapp.1Best answer
Senior III
Apr 23, 2025 11:18 AM UTC

@Ghofrane GSOURI

I have created a new workspace and recreated the project from the .ioc file, and it looks like everything is back to normal.

I guess that means something in the workspace's metadata was not valid?

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)

11 replies

Ghofrane GSOURI
ST Technical Moderator
Apr 22, 2025 2:55 PM UTC

Hello @CTapp.1 

First let me thank you for posting.

Could you please provide your IOC.

I 'will be waiting for your feedback.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
CTapp.1
CTapp.1Author
Senior III
Apr 22, 2025 2:59 PM UTC

Thanks for the quick response - file is attached.

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
Ghofrane GSOURI
ST Technical Moderator
Apr 22, 2025 3:35 PM UTC

Hello @CTapp.1 

I used your IOC to generate the code multiple times and each time the build finished without any errors or warnings, and your project architecture did not change.

GhofraneGSOURI_0-1745335969962.png

Let's try to close STM32CubeIDE and STM32CubeMX and go under C:\Users\XXXXXX then delete .stm32cubeide and .stm32cubemx.

THX

Ghofrane 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
CTapp.1
CTapp.1Author
Senior III
Apr 22, 2025 4:07 PM UTC

Thanks - I've tried that, but the results are the same.

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
CTapp.1
CTapp.1Author
Senior III
Apr 22, 2025 4:32 PM UTC

I've just uninstalled and reinstalled CubeIDE (V.1.18.1), but that has also made no difference.

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
Ghofrane GSOURI
ST Technical Moderator
Apr 23, 2025 7:15 AM UTC

Hello @CTapp.1 

Try to use STM32CubeMX 6.14.1 standalone : this is the LINK to download it .

Open your IOC using STM32CubeMX 6.14.1 standalone then generate the code using STM32CubeIDE as shown 

GhofraneGSOURI_0-1745392514667.png

I will be waiting for your feedback.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
CTapp.1
CTapp.1Author
Senior III
Apr 23, 2025 7:51 AM UTC

Hi @Ghofrane GSOURI

The code is generated as expected when using the standalone MX 6.14.1 - the second system_stm32g0xx.c is not generated in the templates folder, and the code builds successfully.

Does this mean there is an issue with the integrated MX in IDE V1.18.1?

Edited to add:

When using the internal MX, an mx.scratch file is left in the project after code generation.

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
Ghofrane GSOURI
ST Technical Moderator
Apr 23, 2025 9:35 AM UTC

Hello @CTapp.1 

Even with the integrated MX in IDE V1.18.1, everything is working correctly. After multiple generation of the code, the build finished with success. There were no changes in the structure of your project and no duplicate files.

GhofraneGSOURI_0-1745400715189.png

It could be an issue related to your environment.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
CTapp.1
CTapp.1Author
Senior III
Apr 23, 2025 9:38 AM UTC

Ok, but how do I find out where the problem is so that I can fix it?

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
CTapp.1
CTapp.1AuthorBest answer
Senior III
Apr 23, 2025 11:18 AM UTC

@Ghofrane GSOURI

I have created a new workspace and recreated the project from the .ioc file, and it looks like everything is back to normal.

I guess that means something in the workspace's metadata was not valid?

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
Associate
Aug 20, 2025 4:18 PM UTC

Manoj1_0-1755706281132.png

I am also facing the same issue. I just excluded the file from the build, and it worked for me.