Skip to main content
CTapp.1
Senior III
Jun 10, 2025 9:41 PM UTC
Question

Duplicate build artefacts with numeric suffixes

Why do I sometimes get duplicated build artefacts with numeric suffixes. For example:

CTapp1_0-1749591385379.png

This affects everything in the output folder (.elf file, .list file, ...).

I have to manually remove them, as "Clean" doesn't (they aren't part of the build).

This topic has been closed for replies.

3 replies

ST Technical Moderator
Jun 11, 2025 10:57 AM UTC

Hello @CTapp.1 

For further investigation of the issue, could you please add more information about the version of STM32CubeIDE, the toolchain version, and attach your project if possible?

BR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Ozone
Principal
Jun 11, 2025 10:59 AM UTC

And even worse, those duplicates use spaces in their file names.

CTapp.1
CTapp.1Author
Senior III
Jun 11, 2025 7:55 PM UTC

@Souhaib MAZHOUD 

This is with version 1.18.1 on macOS, but I have seen it with other versions (including 1.16).

Unfortunately, I am not able to share a project at this time that shows the issue - but I'll come back if I notice it with one that I can share.

Edited to add:

Toolchain version is 13.3 rel1 (but earlier ones were used with older IDE versions).

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)