Skip to main content
Associate III
October 12, 2023
Solved

DSP Installing

I've followed this tutorial to install the DSP libraries on STM32F407 discovery.

Should I keep all the files in the folders in the attached picture? Or only one per folder? (i.e. according to the uController I choose which one to keep)

screen.png

I think I have to delete the IAR and GCC folders, leaving only ARM, am I wrong? And inside this ARM folder should I delete something? What's the difference between b, bf, l and lf?

Thank you all!

    This topic has been closed for replies.
    KDJEM.1
    KDJEM.1Best answer
    ST Technical Moderator
    October 16, 2023

    Hello @luke514 ,

    STM32CubeIDE use GCC compiler, so you need to keep the GCC folder.

    Note that it is necessary, when you use the DSP Lib with STM32CubeIDE, to add the "arm_cortexM4lf_math" library and the path location file which is in a GCC folder (note 6 and 7 in the figure).

    KDJEM1_0-1697444587146.png

    So, you don't need to delete any folder.

    Thank you for your contribution, and please don't hesitate to post a question or to start a discussion:).

    Kaouthar

    To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

    5 replies

    KDJEM.1
    ST Technical Moderator
    October 13, 2023

    Hello @luke514  , 

    Are you using STM32CubeIDE toolchain? 

    Did you get any issue when you added the DSP library as described in this article? 

    Thank you. 

    Kaouthar

    To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
    luke514Author
    Associate III
    October 13, 2023

    Yes I'm using STM32CubeIDE.

    I don't think I had issue when I installed the libraries, but I have yet to use them so if I installed them wrong, I wouldn't know now

    KDJEM.1
    KDJEM.1Best answer
    ST Technical Moderator
    October 16, 2023

    Hello @luke514 ,

    STM32CubeIDE use GCC compiler, so you need to keep the GCC folder.

    Note that it is necessary, when you use the DSP Lib with STM32CubeIDE, to add the "arm_cortexM4lf_math" library and the path location file which is in a GCC folder (note 6 and 7 in the figure).

    KDJEM1_0-1697444587146.png

    So, you don't need to delete any folder.

    Thank you for your contribution, and please don't hesitate to post a question or to start a discussion:).

    Kaouthar

    To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
    luke514Author
    Associate III
    October 20, 2023

    Thank you for the clarification. I found a faster and easier method to install those libraries, that is in the .ioc file of stm32cubeIDE select "Software Packs" - "Select component" and go on from there.

    KDJEM.1
    ST Technical Moderator
    October 20, 2023

    Hi @luke514 ,

    If your request is answered please click on Accept as Solution on the reply which solved your issue or answered your question.

    Thank you for your contribution to the Community :).

    Kaouthar

    To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.