Skip to main content
Associate
Jan 13, 2026 5:08 PM UTC
Question

Difficulty of flash write for NAND flash MX30LF4G28AC using STM32

Hii Community member,

I need technical help from someone who had faced this issue earlier described as below:

I am currently working on STM32H723ZG mcu in which i had interfaced NAND flash of MX30LF4G28AC using FMC peripheral.

As per our hardware test routine, I am checking flash test in which first a block gets erased and then each page is verify whether it is erased or not. Then a dummy buffer of 4096 get writes in a page and then read back into another buffer and comparing them.

 During comparison, my test passes for some pages and fails for some pages within block. When checked for failed pages, it is found that only last byte i.e. 4095th byte is differing. 

Although i had done configuration for 4Gbit model in cubeMx, my test routine is working for 2Gbit model.

I would welcome any suggestion or some guidance point to resolve my issue.

If any code snippet required, i will share on this chat.

@TDK 

2 replies

TDK
Jan 13, 2026 5:34 PM UTC

This sounds like an MPU configuration error. Like it's using a cached value instead of querying the memory again.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
Jan 15, 2026 5:25 AM UTC

Hii @TDK,

Thanks for reply.

Earlier when I was testing 2 Gbit model (MX30LF2G) at that time MPU configuration was not enabled and this issue is not observed.

I declared two global buffer one for writing and one for reading each size of 2048 during testing of 2Gbit model. 

Now, i had increased size to 4096 of both buffer for read and write for 4Gbit model.

I wanted to know why MPU will be needed if buffer size is increased from 2048 to 4096 ? Is it necessary to enable MPU for this operation and if yes then what configuration should be done ?