Skip to main content
Associate
Dec 10, 2024 12:10 PM UTC
Solved

Different hard faults on STM32H562

I have a problem here:
When calling strcat() on a target string with odd length and odd source, the controller goes into hardfault, SCB_UFST_UNALIGNED is set. 

If I deactivate the unaligned trap (SCB_CCR_UNALIGN_TRP == 0), the following happens.

The controller goes into hardfault on calling putchar(), SCB_BFSR_IBUSERR set. Many previous calls to putchar() work fine.

I use CUBEide with GNU Tools for STM32 12.3rel1.
The code has already been compiled for other STM32 derivatives and other versions of GNU Tools, and works fine on these systems.

This topic has been closed for replies.
lorsBest answer
Associate
Dec 12, 2024 11:52 AM UTC

I can't say exactly which action solved the problem, in this code some timers are used, the corresponding interrupt service routines were installed. I deactivated all these timers for the time being. So the problem was elsewhere.

3 replies

lorsAuthor
Associate
Dec 12, 2024 11:22 AM UTC

The Problem is solved.

mƎALLEm
ST Technical Moderator
Dec 12, 2024 11:23 AM UTC

Hello,

Please, put the description of the solution and mark it as solution.

Thanks.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.