Skip to main content
SUpen.1
Associate II
November 16, 2022
Question

Description Resource Path Location Type Unknown referenced nature: fr.ac6.mcu.ide.core.MCUProjectNature. .project /bootloader Unknown Unknown nature Facing this error as attached.

0693W00000WISbxQAH.png0693W00000WIScHQAX.pngKindly help.

This topic has been closed for replies.

3 replies

Bob S
Super User
November 16, 2022

That is a warning, not an error.

Does the IDE build the bootloader if you modify one of the source files? What if you do a "clean" and build? Or do you always get the "nothing to build" message. If the bootloader DOES build when it supposed to, then perhaps just ignore the warning (not an ideal solution).

Which IDE is this? System Workbench? Or CubeIDE on a project imported from System Workbench?

I will not be much help, but that may give people with more in-depth Eclipse knowledge the info they need to help you.

SUpen.1
SUpen.1Author
Associate II
November 18, 2022

I cleaned the project. Still getting this warning.

This is on stmcubeIDE version 1.9.0.

Pavel A.
November 19, 2022

Is this a SW4STM32 project? If yes, convert it (import) to CubeIDE format.